2013-02-28 7:47 AM
Hi,
I'm developing a self powered USB FS Peripheral Only Device. To detect a USB cable connection to Host I assume to use SRQINT bit in OTG_FS_GINTST register.But for some reason I can not initially clear this bit. I wrote a ''1'' init it to no avail. The VBUS level is about 0.8V measured on PA9 (STM32F20xx).I played with GCCFG_VBUSBSEN and GCCFG_VBUSASEN it also did not help.What's wrong?2013-02-28 11:03 PM
Alternatively can someone suggest what is the right way to detect USB cable insertion in self powered USB FS peripheral device?
I still can not see any way to clear SRQINT after power reset before USB cable is connected.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.