2012-11-30 1:07 AM
AN2586 say
s:
Battery backup To retain the content of the Backup registers when VDD is turned off, the VBAT pin can be connected to an optional standby voltage supplied by a battery or another source. The VBAT pin also powers the RTC unit, allowing the RTC to operate even when the main digital supply (VDD) is turned off. The switch to the VBAT supply is controlled by the power down reset (PDR) circuitry embedded in the Reset block. If no external battery is used in the application, it is highly recommended to connect VBATexternally to VDD.
I made test
s with a 1N
4448
Diode conn
ecte
d to Vbat
, so that an optional Battery can be used for certain applications.
Are there any concerns about using a Diode instead a direct connect to VDD?
Regards
We
rner
#vbat2012-11-30 6:49 AM
You shouldn't have any problems. I use a pair of 1N4448s as steering diodes to run Vbat from Vdd when powered, or from a supercap when not powered. The diode is actually a benefit; it keeps the Vbat volatge below Vdd due to voltage drop across the diode.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.