2009-01-29 7:14 AM
FAT system and SD Card, ARM STM32F103RBT
2011-05-17 3:58 AM
Check this thread:
http://www.st.com/mcu/forums-cat-6318-23.html&start=10 It works quite well!2011-05-17 3:58 AM
Hello,
I`m using ARM STM32F103RBT6. I`m able to record and read data in SD Card with a raw format(Using simple SPI). But I have to use the FAT system because after recorded the card will be read on a PC. Anyone have any library, documentation or example using FAT to help me? Thanks, VinÃcius2011-05-17 3:58 AM
I've post working example hire:
http://www.st.com/mcu/forums-cat-7702-23.html&start=102011-05-17 3:58 AM
Quote:
On 12-01-2009 at 20:40, Anonymous wrote: Check this thread: http://www.st.com/mcu/forums-cat-6318-23.html&start=10 It works quite well! I tried your Code :-[ . First I had to change all ''SPI_FLAG_TXE'' to ''SPI_I2S_FLAG_TXE'' After that I was able to compile the code. But Didn't Work, I start the debug and the CrossStudio tell: Error reading Memory. Someone has any idea to make this code works?Has it? [ This message was edited by: vinicius_acvasconcelos on 14-01-2009 19:32 ] [ This message was edited by: vinicius_acvasconcelos on 14-01-2009 19:34 ]2011-05-17 3:58 AM
Quote:
On 13-01-2009 at 09:22, Anonymous wrote: I've post working example hire: http://www.st.com/mcu/forums-cat-7702-23.html&start=10 Thanks for the example:-D. I tried your exemple, but the CrossStudio give a message: 'printf.c:(.text+0x30): undefined reference to `__putchar' Its the only problem, all the rest seems to work pretty well. Could you have any idea how can I solve this problem?2011-05-17 3:58 AM
Read this:
http://www.rowley.co.uk/documentation/arm_1_7/hcc_customizing_putchar.htm
[ This message was edited by: slawcus on 15-01-2009 23:21 ]2011-05-17 3:58 AM
Quote:
On 15-01-2009 at 23:21, Anonymous wrote: Read this:http://www.rowley.co.uk/documentation/arm_1_7/hcc_customizing_putchar.htm
[ This message was edited by: slawcus on 15-01-2009 23:21 ] Thanks!:-D Its solve the putchar problem, now I'm can compile the code. Today I will test with the Sd Card, and will see if the code realy works.2011-05-17 3:58 AM
Quote:
On 13-01-2009 at 09:22, Anonymous wrote: I've post working example hire: http://www.st.com/mcu/forums-cat-7702-23.html&start=10 I Fixed the __Putchar problem, but your code give a HardwareFault Excepition. What I have to do to this write the data on SD Card in Fat System??? :o2011-05-17 3:58 AM
I'm problem, not function fat file system examples.
Please help! :(We’re moving the ST Community to a new platform to give you a better and more reliable community experience.