2025-08-04 10:09 AM
Hi,
I'm planning to use STM32H562ZI as I3C controller with an I3C v1.0 compatible Target endpoint. Since STM32 I3C IP supports I3C v1.1.1, will there be any potential issues on RSTDAA, ENTDAA, I3C Private Write, I3C Private Read or other electrical parameters with v1.0 ? Though I do not see any limitation based on v1.0 & v1.1.1 specifications (Apart from IBI mandatory byte and new CCCs), I'd like to hear from the community. Appreciate the help.
Thanks,
Srinath
Solved! Go to Solution.
2025-08-10 4:50 AM
ST team reached out directly and STM32H562ZI is backward compatible with I3C v1.0.
This can be marked as resolved now.
2025-08-05 11:31 AM
Hi @srinathkp
This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.
Regards,
Billy
2025-08-10 4:50 AM
ST team reached out directly and STM32H562ZI is backward compatible with I3C v1.0.
This can be marked as resolved now.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.