2016-04-16 6:05 AM
By RM0090 Reference manual, the time can work in ''external clock source mode 1'' mode. That is, the timer can be clocked by 'TIx' input. But I *can't* figure out how to configure it using cubeMX. For example, if I set TIM8's slave mode to ''External Clock Mode 1'', and set the trigger source to ''TI1FP1'', but the ''Channel1'' is grayed. The result is, I can't set CC1S! So 'External clock source mode 1' is hidden by STM32CubeMX actually.
My target MCU is STM32F429IGx.2016-04-18 4:13 AM
Hi diverger,
It’s not a CubeMx problem. You are making the wrong configuration there.As mentioned in the reference manual
, in “Clock selection� -> external clock source mode1 part, page 526:“…..
4. Configure the timer in external clock mode 1 by writing SMS=111 in the TIMx_SMCR
register.
5. Select TI2 as the trigger input source by writing TS=110 in the TIMx_SMCR register.
…�
Setting TS=110 means selecting TI2FP2 as trigger source, but you are selection TI1FP2 instead.
-Hannibal-
2016-04-18 10:55 PM
Thanks, I'll give it a try.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.