2024-02-06 2:38 AM - edited 2024-02-06 4:02 AM
Hello,
I wonder if it is or it is not possible to use more than one ADC independet of each other. My problem is as follows: I want to use ADC1 and ADC2 in independent scan conversion nothing works anymore. My code work for ADC1 alone or ADC2 alone,
uint32_t courant1;// TENSION VIA LE CAPTEUR
uint32_t courant2;// TENSION VIA LE CAPTEUR
/* Private variables ---------------------------------------------------------*/
ADC_HandleTypeDef hadc2;
ADC_HandleTypeDef hadc3;
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_ADC2_Init(void);
static void MX_ADC3_Init(void);
/* USER CODE BEGIN PFP */
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc)
{
if (hadc->Instance == ADC3)
{
courant1=HAL_ADC_GetValue(&hadc3)*20.5/4096;
HAL_ADC_Start_IT(&hadc3);
}
if (hadc->Instance == ADC2)
{
courant2=HAL_ADC_GetValue(&hadc2)*20.5/4096;
HAL_ADC_Start_IT(&hadc2);
}
}
int main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_ADC2_Init();
MX_ADC3_Init();
/* USER CODE BEGIN 2 */
HAL_ADC_Start_IT(&hadc2);
HAL_ADC_Start_IT(&hadc3);
while (1)
{
}
}
/**
* @brief System Clock Configuration
* @r
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Configure the main internal regulator output voltage
*/
__HAL_RCC_PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE3);
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
RCC_OscInitStruct.PLL.PLLM = 16;
RCC_OscInitStruct.PLL.PLLN = 336;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV4;
RCC_OscInitStruct.PLL.PLLQ = 2;
RCC_OscInitStruct.PLL.PLLR = 2;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
{
Error_Handler();
}
}
/**
* @brief ADC2 Initialization Function
* None
* @retval None
*/
static void MX_ADC2_Init(void)
{
/* USER CODE BEGIN ADC2_Init 0 */
/* USER CODE END ADC2_Init 0 */
ADC_ChannelConfTypeDef sConfig = {0};
/* USER CODE BEGIN ADC2_Init 1 */
/* USER CODE END ADC2_Init 1 */
/** Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)
*/
hadc2.Instance = ADC2;
hadc2.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV4;
hadc2.Init.Resolution = ADC_RESOLUTION_12B;
hadc2.Init.ScanConvMode = DISABLE;
hadc2.Init.ContinuousConvMode = ENABLE;
hadc2.Init.DiscontinuousConvMode = DISABLE;
hadc2.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
hadc2.Init.ExternalTrigConv = ADC_SOFTWARE_START;
hadc2.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc2.Init.NbrOfConversion = 1;
hadc2.Init.DMAContinuousRequests = DISABLE;
hadc2.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
if (HAL_ADC_Init(&hadc2) != HAL_OK)
{
Error_Handler();
}
/** Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time.
*/
sConfig.Channel = ADC_CHANNEL_1;
sConfig.Rank = 1;
sConfig.SamplingTime = ADC_SAMPLETIME_15CYCLES;
if (HAL_ADC_ConfigChannel(&hadc2, &sConfig) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN ADC2_Init 2 */
/* USER CODE END ADC2_Init 2 */
}
static void MX_ADC3_Init(void)
{
/* USER CODE BEGIN ADC3_Init 0 */
/* USER CODE END ADC3_Init 0 */
ADC_ChannelConfTypeDef sConfig = {0};
/* USER CODE BEGIN ADC3_Init 1 */
/* USER CODE END ADC3_Init 1 */
/** Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)
*/
hadc3.Instance = ADC3;
hadc3.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV4;
hadc3.Init.Resolution = ADC_RESOLUTION_12B;
hadc3.Init.ScanConvMode = DISABLE;
hadc3.Init.ContinuousConvMode = ENABLE;
hadc3.Init.DiscontinuousConvMode = DISABLE;
hadc3.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
hadc3.Init.ExternalTrigConv = ADC_SOFTWARE_START;
hadc3.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc3.Init.NbrOfConversion = 1;
hadc3.Init.DMAContinuousRequests = DISABLE;
hadc3.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
if (HAL_ADC_Init(&hadc3) != HAL_OK)
{
Error_Handler();
}
/** Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time.
*/
sConfig.Channel = ADC_CHANNEL_10;
sConfig.Rank = 1;
sConfig.SamplingTime = ADC_SAMPLETIME_3CYCLES;
if (HAL_ADC_ConfigChannel(&hadc3, &sConfig) != HAL_OK)
{
Error_Handler();
}
}
static void MX_GPIO_Init(void)
{
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}
Solved! Go to Solution.
2024-02-06 7:16 AM - edited 2024-02-06 8:15 AM
Hello,
If you comment HAL_ADC_Start_IT(&hadc2);, ADC3 works fine. Also if you increase the two sampling rates it works well. So now I'm pretty sure it's due to CPU load that manages two interrupts at higher frequency.
Attached your project on which I modified the reading using DMA and it's working fine.
Hope it helps you.
2024-02-06 2:43 AM
Use this button to properly post source code:
To get that extra row of icons, press this button:
2024-02-06 3:07 AM
Hello,
Better to attach your .ioc file.
2024-02-06 3:23 AM - edited 2024-02-06 3:24 AM
i have changed the sampling time of the Adc2 to 480 cycle and i let the adc3 sampling time at 3 cycle .with this new setting they work well together... but i didn't understand how sampling time could affect the work of 2 ADC in Independent mode..
2024-02-06 3:28 AM - edited 2024-02-06 3:30 AM
It could be something related to the CPU load which is managing two interrupts at the same time of ADC2 and ADC3 with lower sampling rates. By increasing one of the ADC sampling rate you decreased the CPU load.
So better to use DMA instead of interrupt in this case.
2024-02-06 3:30 AM
the same problème i have when i used DMA..
2024-02-06 3:31 AM
DMA with interrupt?
2024-02-06 3:32 AM
@kkhli.1 wrote:i didn't understand how sampling time could affect the work of 2 ADC in Independent mode..
More likely that it affects something(s) in the operation of your code rather than the operation of the ADCs themselves...
2024-02-06 3:35 AM
nonfirst i just called
Hal_adc_start_Dma(hadc2.....) ;et Hal_adc_start_Dma(hadc3....)
but Always one of them work
2024-02-06 3:38 AM
Please share your project at least ioc file so the community members can help you in efficient way.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.