2018-05-10 5:30 AM
I'm developing an HID USB Host application. I have already opened a discussion (
https://community.st.com/0D50X00009XkX0ASAV
) about HID USB Host and I applied all the suggested patches in forum, but now I have another problem.When I try to send data to device (is a HID custom device that work fine if connected to PC) with SBH_HID_SetReport() function, it return 'USBH_BUSY' every time I try to send message.
The problem seems to be inside the USBH_HandleControl() function: the state machine reaches the 'CTRL_DATA_OUT_WAIT' state but, when it call USBH_LL_GetURBState(), return 'USBH_URB_STALL' status and than the USBH_HID_SetReport() function return 'USBH_BUSY'.This is the code used to send data:
&sharpdefine MAX_USBDATASIZE (64)
.
.
.
static uint8_t USBBufToSend[MAX_USBDATASIZE];
static uint16_t lenUSBBufToSend;
.
.
.
USBH_StatusTypeDef res;.
.
.
res=USBH_HID_SetReport(&hUsbHostFS,0x02,0x00,USBBufToSend,lenUSBBufToSend);
Why the device state is 'USBH_URB_STALL'? Is it my mistake?
Is possible to resume the correct state?null2018-08-10 9:34 AM
Sorry, bumping old zombie unanswered threads off my feed
2024-08-14 12:04 PM
Great support lol!! Can't help, bump it off! What a totally unprofessional mess ST USB driver is!
IMHO ST MCU business won't last much longer given all the competition such as Raspberry Pi and ESP industrial boards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.