2016-01-28 11:14 PM
Hi.
I have been playing with Cube for the Nucleo F1 series, and I'm interested in getting a USB app running. I know a little about HID, and I can create a HID cube project for SW4STM32 and it enumerates as a HID. The problem is when I create a cube project but this time for a CDC device, I find it wont complete the enumeration, and instead Device Manager shows the dreaded exclamation icon, and interestingly this icon is next to a not yet working Com Port (x), in this case 12. The driver properties within device Manager give the error: This device cannot start (Code 100 A device which does not exist was specified. Does this mean that ST have not completed the descriptor tables? It seems to be ok for a plain old HID device, has anyone come up with this before? Cheers kvresto2016-01-29 2:10 PM
ST's CDC device firmware works perfectly well on the STM32F405 and STM32F072, so I don't see why it wouldn't work on an F1. Try fiddling with the build configuration, in the context of the hardware implementation (turn on/off Vbus, for example).
I should add that when I say the CDC device firmware ''works'', I mean that out of the box all it does is enumerate as a virtual COM port under Windows. You have to write your own firmware that interacts with ST's API to allow you to ship data between the MCU and PC.2016-01-29 3:06 PM
Thanks Mark. I have put an order in for a STM32F072 discovery. My board is an older Olimex p103, I don't actually own any other STM32 dev board, although I 'll keep playing with it, based on your comments, its got to be my project set up in some way.
Cheers2016-01-30 3:43 PM
My STM32F072B discovery arrived and I repeated exactly what I have already done previously. I created a USB CDC device project in cube, selected the STM32F072B discovery within board selector and when the project opened up, I then enabled USB Device FS, and selected the Virtual Com Port from the USB_DEVICE selection. Downloaded, and still no joy, it wont enumerate correctly. I have included a pic of device manager. Is there some other setting I'm missing? When I do the same for a HID device, I have no problem it enumerates correctly as a HID???????
cheers kvresto ________________ Attachments : cdc-device.jpg : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0au&d=%2Fa%2F0X0000000bat%2FZdIqZQCohiQNrG5NXFtXolcoBNJypluF4dyOX3lzGlw&asPdf=false2016-01-30 7:45 PM
Hi kvresto,
On your Windows PC, there is trouble on the registry around the STM32 VCP device, which disturbs unified recognition of the pair of CDC interfaces (Control / Data interfaces). And then, each interface is registered as separate instance on the registry. 1) Clean up the VCP instances in trouble on your PC using USBDeview utility,http://www.nirsoft.net/utils/usb_devices_view.html
- Run this utility - Scroll the list to left, show up '' Vendor ID'' column - Click on '' Vendor ID'' label --> the list is sorted by VID/PID - Find VID/PID = 0483/5740 (in hexadecimal, 1155/22336 in decimal, shown on the source code) - (shift-)click on the all lines of this VID/PID to select them - right click on selected lines and choose '' Uninstall the selected devices'' 2) To make sure your device as CDC one, fix the bDeviceClass field of the Device descriptorusbd_desc.c line: 119
/* USB Standard Device Descriptor */
__ALIGN_BEGIN uint8_t USBD_FS_DeviceDesc[USB_LEN_DEV_DESC] __ALIGN_END =
{
0x12, /*bLength */
USB_DESC_TYPE_DEVICE, /*bDescriptorType*/
#if (USBD_LPM_ENABLED == 1)
0x01, /*bcdUSB */ /* changed to USB version 2.01
in order to support LPM L1 suspend
resume test of USBCV3.0*/
#else
0x00, /* bcdUSB */
#endif
0x02,
// 0x00, /*bDeviceClass*/
0x02, /*bDeviceClass*/ // <-----------
3) Plug in revised CDC device to the PC, and wait for automatic driver download from Windows Update,
OR
you may pre-install ST VCP driver, distributed on this page,
http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1533/PF257938
You'll need to run DPINST utility in the folder explicitly, to make the driver (INF) pre-installed. C:\Program Files\STMicroelectronics\Software\Virtual comport driver\Win7\dpinst_xexe or dpinst_amdexe Tsuneo2016-01-31 2:06 PM
Hi Tsuneo.
That's the trick, it worked. Thanks for your expert advice. I preinstalled the ST driver which I didn't do previously, and enumeration went through perfectly. cheers kvrestoWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.