2025-04-08 4:17 PM - last edited on 2025-04-16 7:17 AM by FBL
Hi,
I want to start using the STM32U073KCU6 MCU in an upcoming product but don't have a ton of familiarity with STM MCUs.
My attraction to the device is based around the integrated USB functionality and I am trying to figure out if it can be field programed using the USB lines only (and of course being powered on).
What do I need to do in my pcb to make sure this is possible? what software tools (command line scripts or otherwise) do you recommend for this programming step?
Best,
Teva
2025-04-16 9:25 AM
Hi @teva
> field programed using the USB lines
You mean DFU IAP application? Check this firmware example using STM32G0 and MB1933 schematics to interface USB peripheral on U083 discovery kit.
Getting started with STM32U0 MCUs hardware development application note should be helpful.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-04-16 9:40 AM - edited 2025-04-16 9:41 AM
I'm thinking the question is more about if the System Loader supports "STM32 DEVICE" type DFU programming with tools like STM32 Cube Programmer. Per AN2606
2025-06-05 7:56 PM
Yeah thats right. Specifically what i want is the ability to have application code running over USB CDC and the ability to flash it over the same lines without reset (It looks like DFU is the main option for this),
2025-06-09 4:11 AM
First, configure the USB device as a composite class to enable both CDC communication and DFU for firmware updates. Ensure endpoints are assigned to each class. Next, implement a software mechanism to trigger a jump to the system loader, to enter DFU mode.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.