2008-05-06 10:22 PM
USB Enumeration Failure detection and Inverted USART
2011-05-17 3:34 AM
Hello everyone,
I got two questions where I require some help. 1) Is there a way to detect a failed usb enumeration? Think of a situation where 5 units of power is drawn to be drawn on Vbus, for a bus-powered device. Incase the host is unable to provide this, the power drawn has to be downed to 1 unit. 2) Is it possible to have the USART1 Rx, Tx pins inverted? Think of a logic inverter connected to the Rx and Tx pins. This same thing done in either hardware or software without external components. Thank you for your time. -Mad D2011-05-17 3:34 AM
Ummm... No replies still :o
STOne-32, Lanchon... do you at least have any ideas? -Mad D2011-05-17 3:34 AM
I'm sorry, I don't know the first thing about USB. I believe that you need to expose two or more different configurations in the descriptors and have the host choose.
I don't know the USART peripheral. (Of course you could do that by bit banging in GPIO mode.)2011-05-17 3:34 AM
Thanks for the reply lanchon.
USART: The SIR turned out to work the way I want... But unfortunately, the pulse width in IrDa is 3/16 of the baud! I'm now trying to see whether a 10 step PWM signal would work. Unlike bit banging on a GPIO, in a 10 step PWM you can set the next step before hand according to the ST docs. I haven't got this to work yet and dont know how much better/efficient it is. But if someone has worked with it, please let me know. USB: Mystery indeed! -Mad DWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.