2017-11-13 1:32 AM
Hi,
i wanted to establish a connection from a STM32F070CB as a device to my PC via USB. So first i simply wanted to use the code generated by CubeMX since with the precompiled code the device should be identified properly on the PC. But i just get the message: USB deivce not recognized
I use a crystal with 12 MHz and the clock config is adapted properly.
The device is powered over USB and connected according to AN4879. Which means neither D+ nor D- have a pull up or pulldown since as far as i know this is only necessary for High-Speed USB.
I already increased heap & stack size and added a delay before MX_USB_Dvice_Init().
If any one has an idea what the problem could be i'll be very thankfull.
Cheers
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.