2014-04-25 11:49 AM
2014-04-25 12:18 PM
I get the Tx interrupt but when I call the void USART_SendData(USART_TypeDef* USARTx, uint16_t Data) , the USARTx-> DR register does not reflect the value it is assigned.
Why would it? It's not a memory cell, it's a peripheral register whose behaviour is different in the read and write contexts because it's pointing at a complete different set of flip-flops. If you stick the debugger over the USARTx->DR you will break it, and the status reported in USARTx->SR2014-04-25 1:27 PM
Hi Clive,
Thanks for replying.I cannot see any data on the oscilloscope. The TXE bit in the SR register is always set.If i try loop back by connecting Tx to Rx i do not get any Rx interrupt either.2014-04-25 8:15 PM
RCC_APB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE);
AHB1 AHB12014-04-25 8:24 PM
// STM32 USART IRQ TX/RX Loop (USART3 Tx PB.10, Rx PB.11) STM32F4 Discovery - sourcer32@gmail.com
#include ''stm32f4_discovery.h''
volatile char StringLoop[] = ''The quick brown fox jumps over the lazy dog
'';
/**************************************************************************************/
void RCC_Configuration(void)
{
/* --------------------------- System Clocks Configuration -----------------*/
/* USART3 clock enable */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART3, ENABLE);
/* GPIOB clock enable */
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE);
}
/**************************************************************************************/
void GPIO_Configuration(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
/*-------------------------- GPIO Configuration ----------------------------*/
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10 | GPIO_Pin_11;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOB, &GPIO_InitStructure);
/* Connect USART pins to AF */
GPIO_PinAFConfig(GPIOB, GPIO_PinSource10, GPIO_AF_USART3);
GPIO_PinAFConfig(GPIOB, GPIO_PinSource11, GPIO_AF_USART3);
}
/**************************************************************************************/
void USART3_Configuration(void)
{
USART_InitTypeDef USART_InitStructure;
/* USARTx configuration ------------------------------------------------------*/
/* USARTx configured as follow:
- BaudRate = 9600 baud
- Word Length = 8 Bits
- One Stop Bit
- No parity
- Hardware flow control disabled (RTS and CTS signals)
- Receive and transmit enabled
*/
USART_InitStructure.USART_BaudRate = 9600;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
USART_Init(USART3, &USART_InitStructure);
USART_Cmd(USART3, ENABLE);
USART_ITConfig(USART3, USART_IT_TXE, ENABLE);
USART_ITConfig(USART3, USART_IT_RXNE, ENABLE);
}
/**************************************************************************************/
void NVIC_Configuration(void)
{
NVIC_InitTypeDef NVIC_InitStructure;
/* Configure the NVIC Preemption Priority Bits */
NVIC_PriorityGroupConfig(NVIC_PriorityGroup_0);
/* Enable the USART3 Interrupt */
NVIC_InitStructure.NVIC_IRQChannel = USART3_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
}
/**************************************************************************************/
void USART3_IRQHandler(void)
{
static int tx_index = 0;
static int rx_index = 0;
if (USART_GetITStatus(USART3, USART_IT_TXE) != RESET) // Transmit the string in a loop
{
USART_SendData(USART3, StringLoop[tx_index++]);
if (tx_index >= (sizeof(StringLoop) - 1))
tx_index = 0;
}
if (USART_GetITStatus(USART3, USART_IT_RXNE) != RESET) // Received characters modify string
{
StringLoop[rx_index++] = USART_ReceiveData(USART3);
if (rx_index >= (sizeof(StringLoop) - 1))
rx_index = 0;
}
}
/**************************************************************************************/
int main(void)
{
RCC_Configuration();
GPIO_Configuration();
NVIC_Configuration();
USART3_Configuration();
while(1); // Don't want to exit
}
/**************************************************************************************/
2014-04-29 2:57 PM
Thanks for spotting that Clive.
2015-04-06 2:34 PM
shouldn't the interrupt handler also handle other interrupt sources?
The interrupt handler only handles the RXNE and the TXE interrupt. But setting RXNEIE also enables the ORE interrupt. In your example, the interrupt might jam when the ORE interrupt is not serviced. An other solution is to add the following to the USART init function: //Disable overrun detection by forcing ORE to zero USART_OverrunDetectionConfig(USART3, USART_OVRDetection_Disable); Best regardsWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.