2015-04-05 11:30 PM
I was able to toggle gpio PA0 & PA13 , but when I try to do the same using PA1 & PA2 I'm not seeing any changes on these pins (used an oscilloscope to monitor).
When I checked the schematic I could find these pins are connected to the interrupt pins of Accelrometer L3GD20 , Is this causing the problem or did my pins got damaged ? #discovery #stm32f4292015-04-06 7:40 AM
Well if it's driving the pins it's going to cause a conflict. Perhaps you can configure them in a tri-stated mode, or simply remove the chip?
2015-04-06 9:15 PM
Thnaks for the reply,
Well I cant remove the chip since the board is owned by someone else, I want to know whether the pin got dmaged or is the pin not responding since acclerometer is driving it ?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.