2014-05-25 5:23 PM
Hello, I am having a problem with my STM32F4 USART2. the problem is throwing me this bullshit and can not find where the error may be.
#include ''stm32f4xx.h'' // Device header#include ''stm32f4xx_gpio.h''#include <misc.h> // I recommend you have a look at these in the ST firmware folder#include ''stm32f4xx_usart.h''#include ''stm32f4xx_rcc.h''#include <stdio.h>#include <stdlib.h>#include <string.h>#include <stdint.h>int flag = 0;void init(USART_TypeDef* USARTx, uint32_t baudrate) { GPIO_InitTypeDef GPIO_InitStruct; USART_InitTypeDef USART_InitStruct; NVIC_InitTypeDef NVIC_InitStructure; //General settings of pins TX/RX GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStruct.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStruct.GPIO_OType = GPIO_OType_PP; GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_UP; if(USARTx == USART1){ RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE); RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE); GPIO_InitStruct.GPIO_Pin = GPIO_Pin_6 | GPIO_Pin_7; // Pins B6 (TX) and B7 (RX) GPIO_Init(GPIOB, &GPIO_InitStruct); GPIO_PinAFConfig(GPIOB, GPIO_PinSource6, GPIO_AF_USART1); GPIO_PinAFConfig(GPIOB, GPIO_PinSource7, GPIO_AF_USART1); NVIC_InitStructure.NVIC_IRQChannel = USART1_IRQn; } else if(USARTx == USART2){ flag =1; RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2, ENABLE); RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE); GPIO_InitStruct.GPIO_Pin = GPIO_Pin_2 | GPIO_Pin_3; // Pins A2 (TX) and A3 (RX) GPIO_Init(GPIOA, &GPIO_InitStruct); GPIO_PinAFConfig(GPIOA, GPIO_PinSource2, GPIO_AF_USART2); GPIO_PinAFConfig(GPIOA, GPIO_PinSource3, GPIO_AF_USART2); NVIC_InitStructure.NVIC_IRQChannel = USART2_IRQn; } else if(USARTx == USART3){ RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART3, ENABLE); RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD, ENABLE); GPIO_InitStruct.GPIO_Pin = GPIO_Pin_8 | GPIO_Pin_9; // Pins D8 (TX) and D9 (RX) GPIO_Init(GPIOD, &GPIO_InitStruct); GPIO_PinAFConfig(GPIOD, GPIO_PinSource8, GPIO_AF_USART3); GPIO_PinAFConfig(GPIOD, GPIO_PinSource9, GPIO_AF_USART3); NVIC_InitStructure.NVIC_IRQChannel = USART3_IRQn; } else if(USARTx == UART4){ RCC_APB1PeriphClockCmd(RCC_APB1Periph_UART4, ENABLE); RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE); GPIO_InitStruct.GPIO_Pin = GPIO_Pin_10 | GPIO_Pin_11; // Pins C10 (TX) and C11 (RX) GPIO_Init(GPIOC, &GPIO_InitStruct); GPIO_PinAFConfig(GPIOC, GPIO_PinSource10, GPIO_AF_UART4); GPIO_PinAFConfig(GPIOC, GPIO_PinSource11, GPIO_AF_UART4); NVIC_InitStructure.NVIC_IRQChannel = UART4_IRQn; } else if(USARTx == UART5){ RCC_APB1PeriphClockCmd(RCC_APB1Periph_UART5, ENABLE); RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE); RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD, ENABLE); GPIO_InitStruct.GPIO_Pin = GPIO_Pin_12; // Pin C12 (TX) GPIO_Init(GPIOC, &GPIO_InitStruct); GPIO_InitStruct.GPIO_Pin = GPIO_Pin_2; // Pin D2 (RX) GPIO_Init(GPIOD, &GPIO_InitStruct); GPIO_PinAFConfig(GPIOC, GPIO_PinSource12, GPIO_AF_UART5); GPIO_PinAFConfig(GPIOD, GPIO_PinSource2, GPIO_AF_UART5); NVIC_InitStructure.NVIC_IRQChannel = UART5_IRQn; } else if(USARTx == USART6){ RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART6, ENABLE); RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE); GPIO_InitStruct.GPIO_Pin = GPIO_Pin_6 | GPIO_Pin_7; // Pins C6 (TX) and C7 (RX) GPIO_Init(GPIOC, &GPIO_InitStruct); GPIO_PinAFConfig(GPIOC, GPIO_PinSource6, GPIO_AF_USART6); GPIO_PinAFConfig(GPIOC, GPIO_PinSource7, GPIO_AF_USART6); NVIC_InitStructure.NVIC_IRQChannel = USART6_IRQn; } //UART setting USART_InitStruct.USART_BaudRate = baudrate; USART_InitStruct.USART_WordLength = USART_WordLength_8b; // octet comme taille élémentaore (standard) USART_InitStruct.USART_StopBits = USART_StopBits_1; // bit de stop = 1 (standard) USART_InitStruct.USART_Parity = USART_Parity_No; // pas de bit de parité (standard) USART_InitStruct.USART_HardwareFlowControl = USART_HardwareFlowControl_None; // pas de controle de flux (standard) USART_InitStruct.USART_Mode = USART_Mode_Tx | USART_Mode_Rx; USART_Init(USARTx, &USART_InitStruct); USART_ITConfig(USARTx, USART_IT_RXNE, ENABLE); //Setting of interrupt NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); //Enable UART USART_Cmd(USARTx, ENABLE); }void send_char(USART_TypeDef* USARTx, unsigned char c) { USART_SendData(USARTx, c); while (USART_GetFlagStatus(USARTx, USART_FLAG_TXE) == RESET) { } }void Delay(__IO uint32_t nCount){ while(nCount--) {}}void LED() { GPIO_InitTypeDef GPIO_InitStructure; RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD,ENABLE); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_12 | GPIO_Pin_13 | GPIO_Pin_14 | GPIO_Pin_15; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ; GPIO_Init(GPIOD, &GPIO_InitStructure);}int main(){ init(USART2,9600); Delay(0x5FFFFF); LED(); send_char(USART2, 'A'); Delay(0x5FFFFF); send_char(USART2, 'B'); Delay(0x5FFFFF); send_char(USART2, 'C'); while(1) { if (flag ==1){ GPIO_SetBits(GPIOD, GPIO_Pin_12 | GPIO_Pin_13 | GPIO_Pin_14 | GPIO_Pin_15); Delay(0x5FFFFF); GPIO_ResetBits(GPIOD, GPIO_Pin_12 | GPIO_Pin_13 | GPIO_Pin_14 | GPIO_Pin_15); Delay(0x5FFFFF); } }}regards2014-05-25 6:41 PM
Hello, I am having a problem with my STM32F4 USART2. the problem is throwing me this bullshit and can not find where the error may be.
Sorry, I'm not sure what that means in terms of functionality. Do other USART work? How are you attempting to wire up? What is/is not working? Can you see signals with a scope?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.