2014-11-18 5:33 AM
I have STM32RBT6. After initialisation of USART1, the RTS remains high. The code is as follows:
/** USART1 GPIO Configuration
PA9 ------> USART1_TX PA10 ------> USART1_RX PA11 ------> USART1_CTS PA12 ------> USART1_RTS */ GPIO_InitTypeDef GPIO_InitStruct; USART_InitTypeDef usartinit; NVIC_InitTypeDef NVIC_InitStructure; /* System Clocks Configuration */ /* USART1 clock enable */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE); /* GPIOA clock enable */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE); /*Enable APB2 peripheral clock */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE); /* Configure USART1 RTS and USART1 Tx as alternate function push-pull */ GPIO_InitStruct.GPIO_Pin = GPIO_Pin_9 | GPIO_Pin_12; GPIO_InitStruct.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_Init(GPIOA, &GPIO_InitStruct);// Override RTS ToDo: check for bug in RTS handling !!!!!!!!!!!!!!!!!!!!!!!!! GPIO_InitStruct.GPIO_Pin = GPIO_Pin_12; GPIO_InitStruct.GPIO_Mode = GPIO_Mode_Out_PP; GPIO_Init(GPIOA, &GPIO_InitStruct); GPIO_ResetBits(GPIOA, GPIO_Pin_12); /* Configure USART1 CTS and USART1 Rx as input floating */ GPIO_InitStruct.GPIO_Pin = GPIO_Pin_11 | GPIO_Pin_10; GPIO_InitStruct.GPIO_Mode = GPIO_Mode_IN_FLOATING; GPIO_Init(GPIOA, &GPIO_InitStruct); /* Configure USART1, 115200 baud, harware flow control, 1 stop bit, no parity */ usartinit.USART_BaudRate = 115200; usartinit.USART_HardwareFlowControl = USART_HardwareFlowControl_RTS_CTS; usartinit.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; usartinit.USART_Parity = USART_Parity_No; usartinit.USART_StopBits = USART_StopBits_1; usartinit.USART_WordLength = USART_WordLength_8b; USART_Init(USART1, &usartinit); USART_Cmd(USART1, ENABLE); /* Enable USART1 IRQ */ NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannel = USART1_IRQn; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); USART_ITConfig(USART1, USART_IT_RXNE, ENABLE); // enable IRQ on RX NVIC_EnableIRQ(USART1_IRQn); // Enable IRQ for USART1 in NVIC I am using STM32F10x Standard Peripherals Library 3.5.1What am I missing?Regards,Marko #stm32-usart-rts-remains-high2014-11-18 9:21 AM
What do you have attached to the pin?
In GPIO mode you should be able to drive up/down. In AF mode, you might want to double check the errata, seem to recall one of the CTS/RTS grouping clashing with CAN, requiring CAN to be remapped elsewhere.2014-11-18 3:31 PM
Thank you. The issue is described in errata. CAN must be remapped to alternate location even when not used.
http://www.st.com/st-web-ui/static/active/en/resource/technical/document/errata_sheet/CD00190234.pdfWorkaround from section 2.8.1:When USART1_RTS is used, the CAN must be remapped to either another IO configuration when the CAN is used, or to the unused configuration (CAN_REMAP[1:0] set to “01�?) when the CAN is not used.Regards,MarkoWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.