cancel
Showing results for 
Search instead for 
Did you mean: 

Does emWin surpport LCD controller's on-chip font?

Microstar
Associate III
Posted on November 17, 2014 at 08:06

My LCD controller embeds fonts that index by coding.

I'm using STemWin.

I decide to ask here, cause I'm not a emWin commercial user.

#!espn #emwin
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Posted on November 17, 2014 at 14:38

Hi,

We don't really have enough insight into what specifically you are doing, and how. Would you mind giving a little more information about your issue so we can better explain it to our developement team? 

Regards,

Heisenberg.

Microstar
Associate III
Posted on November 18, 2014 at 02:33

OK. 

As we known, we usually use a LCD graphic controller to drive the displayer,

TFT/STN etc.

To display a char in emwin, we use its bitmap. 

So, emwin needs a font lib, inside or outside.

Now, THIS ONE (graphic controller) has fonts embedded.

And, it auto-displays a char's bitmap if I input it's unicode.

This may free the MCU from writing font bitmaps, if I can use THIS with emwin.

Posted on November 18, 2014 at 19:47

Ok, but WHAT controller are you using, perhaps you can cite a data sheet, or something?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Microstar
Associate III
Posted on November 19, 2014 at 02:10

Though I don't quite understand why you want more about the controller,

I attached as follow.

RA8875 builds in a Serial Flash/ROM interface, supporting for protocol of 4-BUS (Normal Read), 5-BUS (FAST Read), Dual mode 0, Dual mode 1, Mode 0 and Mode 3.Serial Flash/ROM function can be used for FONT mode, DMA mode and Direct Access Mode. FONTmode means that the external serial Flash/ROM is treated as a source of FONT bitmap. To supportthe most useful FONT characters, RA8875 is compatible with the FONT ROM of professional FONTvendor—Genitop Inc.

________________

Attachments :

RA8875_Datasheet_V19_EN.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzWI&d=%2Fa%2F0X0000000bN4%2FyvQdfusO67CQdqaKvuxdNOOfAG0Jaw8TFhChUY2nQtA&asPdf=false
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.