2014-04-05 6:23 PM
I'm using a STM32F3 Discovery and connecting it to labVIEW the problem is that I can't receive more than one byte. Can someone help me modifying my code to allow multiple byte reception. I'm testing it sending something and reading it in labVIEW. A problem occurs when I send more than 1 byte.
//-----------------------------------------------------Register comment format-----------------------------------------------------////[ Register bits ] Function name[ Function bits ] -> Value Effect explanation//---------------------------------------------------------------------------------------------------------------------------------//&sharpinclude <stm32f30x.h>&sharpinclude <stdio.h>&sharpinclude <math.h>&sharpinclude ''lib/delay.h''void charTX ( char ch );void stringTX ( char *string );uint8_t GetChar ( void );char letra;int main ( void ) { char output[4]; delayinit(); //-----------------------------------------------------PC4 Configuration------------------------------------------------------// RCC->AHBENR |= RCC_AHBENR_GPIOCEN; // [ 19 ] IOPCEN = 1 I/O port A clock enabled. GPIOC->MODER |= 2 << ( 4*2 ); // [ 9:8 ] MODER4[ 1:0 ] = 10b Alternate function on // PIN C4 //GPIOC->OTYPER |= 1 << ( 4*1 ); // [ 4 ] OT4 = 1 Output as open drain GPIOC->OSPEEDR |= 3 << ( 4*2 ); // [ 9:8 ] OSPEEDR4[ 1:0 ] = 11b 50 MHz High-speed on PIN C4 //GPIOC->PUPDR &= ~( 3 << ( 4*2 ) ); // [ 9:8 ] PUPDR4[ 1:0 ] = 0 No pull-up/down om PIN C4 GPIOC->AFR[ 0 ] |= 7 << ( 4*4 ); // [ 17:16 ] AFRL4[ 3:0 ] = 0111b AF7( USART1_TX ) on PIN C4 // PC5 configuration (RX)GPIOC->MODER |= 2 << (5*2); // GPIO_Mode_AFGPIOC->AFR[0] |= 7 << (5*4); // AF7 RCC->APB2ENR |= RCC_APB2ENR_USART1EN; // Enable USART1 clock USART1->BRR = 72000000/9600; USART1->CR1 &= ~USART_CR1_OVER8; // Oversampling mode = 16 USART1->CR1 &= ~USART_CR1_M; // Word length = 8 bits USART1->CR1 &= ~USART_CR1_PCE; // No parity USART1->CR1 |= USART_CR1_TE; // Transmitter enable USART1->CR1 |= USART_CR1_RE; // Receiver enable USART1->CR1 |= USART_CR1_UE; // USART enable USART1->CR2 &= ~(USART_CR2_STOP_1 | USART_CR2_STOP_0); // one stop bit for( ;; ) { letra = GetChar() sprintf(output,''%4d\n'',letra); stringTX(output); delaybyms(10); } }void charTX ( char ch ) { while (!(USART1->ISR & USART_ISR_TXE)); USART1->TDR = (ch & 0xFF);}void stringTX ( char *string ){ do { charTX( *string ); *string++; }while(*string);}uint8_t GetChar ( void ) { while (!(USART1->ISR & USART_ISR_RXNE)); return ((uint8_t)(USART1->RDR & 0xFF));} #usart-stm32f32014-04-05 10:44 PM
Ok. But for manipulating data I have to use
USART1->RDR and USART1->TDR ?
2014-04-05 11:00 PM
And so the problem is what exactly? The routines to perform ''getchar'' and ''putchar'' functionality are pretty basic, requiring that you check that something is available, or empty, respectively. They could be implemented in ways which are non-blocking, use buffers, and interrupts, etc.
Have you done much C, and STDIO, type development before?2014-04-05 11:29 PM
Not so much. What string functions do you recommend for me to study
2014-04-06 5:15 PM
You should probably familiarize yourself with all the functions, your can always look up the specific syntax when you need to use them.
http://web.cs.swarthmore.edu/~newhall/unixhelp/C_strings.html
2014-04-06 9:58 PM
Hey Clive. Can you explain me this:
I send 4000 and as a response I receive 4000 so it's fine. But if I see at debugger ch variable (which is the receiver) I see that has a value of 51 (always). Why is that? What kind of conversion do I have to do with ''ch''. I don't get it.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.