2015-02-09 9:27 AM
Hi All,
For my application I need to send 5 bytes over UART repeatedly. I store the 5 bytes in an array (TxBuffer) and iterate through it (index 0-4) on every USART_IT_TXE interrupt. When my counter reaches 5, I disable TX and reset my counter.The issue is that when I do this the last byte is almost always sent as 0xFF (even though I can see the TDR being updated correctly). However, if I step through the code, it sends properly. I've also tried expanding my counter by one, in which case it sends my 5 bytes correctly and then sends 0xFF. I'm assuming I'm missing some sort of timing restriction, but from what I've seen in examples and the datasheet I'm not sure what it is. Here's my interrupt routine: char TxBuffer[TX_LEN] = {''1234''}; #define TX_LEN 5 void USART1_IRQHandler(void) { /* Send UART ---------------------------------------------------------------*/ if(USART_GetITStatus(TEST_COM1, USART_IT_TXE) != RESET) { if (TxCount == TX_LEN){ TxCount = 0; USART_ITConfig(TEST_COM1, USART_IT_TXE, DISABLE); USART_ClearFlag(TEST_COM1, USART_IT_TXE); USART_DirectionModeCmd(TEST_COM1, USART_Mode_Rx, ENABLE); usartOnFlag = 0; } else{ /* Write one byte to the transmit data register */ USART_SendData(TEST_COM1, TxBuffer[TxCount]); TxCount = TxCount + 1; } } }2015-02-09 9:55 AM
TXE is Transmit Buffer Empty, it flags when the the FIRST bit of the LAST byte hits the wire, and the holding buffer for the NEXT byte is empty.
You need to use TC (Transmit Complete), when the LAST bit of the LAST byte has hit the wire.2015-02-09 10:51 AM
Perfect, that was the issue. Thanks!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.