2017-01-11 12:44 AM
Hi, newby here. I recently bought two discovery boards from Conrad.nl.
One with a STM32F100RTB and the other with a STM8S003K3T.
Now I wanted to upgrade the firmware of the integrated ST-LINK modules on the Discovery boards. According to the documentation :
On ST-LINK/V2-1 boards, upgrade firmware to the version V2J28M
On ST-LINK/V2 boards, upgrade firmware to the version V2J28S7.
On ST-LINK boards, upgrade firmware to the version V1J13S4.
But in my case the STM32 board is updated to firmware V1.JS0
And worse, the STM8 board to firmware V1.J0.S4
This version seems to be too old for the ST-LINK Utility.
What am I doing wrong?
Regards,
Wilko Lunenburg
Note: this post was migrated and contained many threaded conversations, some content may be missing.2017-01-12 12:10 PM
you have got the last version of STM32 debug interface but the STM8 debug interface is not supported.
Ah ,that explains it as this ST-Link is integrated on the STM32 board.
Wilko
2017-01-12 12:13 PM
For the STM8 board, the STLink firmware is also upgraded correctly:
That may be so, but the ST-Link utility V4.0.0.0 doesn't want to speak with it saying
'Old STLink firmware detected. Please upgrade it'
And that, I cannot.
Wilko
2017-01-12 12:16 PM
Hi Clive One,
Thanks, I tried it. But it 'upgrades' it to a version lower than the one I already had. And my ST-Link utility (4.0.0.0) doesn't want to spreak with that one either. Do you by any change also have an older ST-Link utillity?
Wilko
2017-01-12 12:23 PM
https://drive.google.com/open?id=0B7OY5pub_GfIOFVzQTV0VEE1TG8
https://drive.google.com/open?id=0B7OY5pub_GfIcUpnMk5yc3g0Yk0
Yes, also 3.0 thru 3.9 but don't have a good grasp of what version of firmware each has.
2017-01-12 12:31 PM
Which board/version are you currently trying to update? I think the V1 stopped at J13, and V2 started at J14
2017-01-13 1:39 AM
Thanks for the older tools, unfortunately both will not work with the board I have (tried it on a clean windows 7 pc) .
The board is a STM8S VL DISCOVERY that I bought last year from Conrad.nl, it is odd that they sell stuff you cannot use...
But I don't think it is worth spending any more of anyone's and my time on it. I have the other STM32-DISCOVERY board with a STM32F103RBT to play with. Thanks to all.
Wilko
2017-01-13 3:50 AM
Hi Wilko,
The STLink utility supports only the STM32 devices.
For your STM8, you should use : STVP (for programming) and the STVD (for debug).You can download those tools from ST website. Just download , it enables you to get the 2 tools simultaneously.Khouloud.
2017-01-13 4:17 AM
ST offers/offered a stand-alone version of the ST-Link for a very affordable price. I got one some years ago for the price of about 3 Discovery boards. Not sure if it's still available and in that price region. And, it's only worthwhile if you want to dig deeper into the STM8 world (i.e. get more boards of that kind).
Otherwise, I would suggest to get another stand-alone debug pod, like the J-Link or a CMSIS-DAP compatible one. They enjoy greater support from different toolchains, and leave you other alternatives (different vendors).
2017-01-13 6:02 AM
Hi Wilko,
You are confusing between:
http://www.st.com/en/development-tools/st-link.html
: anin-circuit debugger and programmer for the STM8 and STM32 microcontroller families.
http://www.st.com/en/embedded-software/stsw-link004.html
:a full-featured software interface for programming STM32 microcontrollers.
Khouloud
2017-01-13 6:05 AM
Hi Avatar,
When I continue with the STM8, a standalone programmer/debugger is what I will buy. But the J-Link (Segger) you suggest, seems not support the STM8. So it will probably be a ST-Link v2.
Wilko
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.