2016-01-28 1:12 PM
--
2016-01-29 2:57 AM
Hi Tulip,
Check the following resources, it will help you a lot to build your project:The application note AN3997 ''Audio playback and recording using the STM32F4DISCOVERY� and the associated firmware.
The STM32Cube application example in “Audio_playback_and_record� under the following path Projects\STM324x9I_EVAL\Applications\Audio.
The last version of STM32CubeF4 is under this
http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1743/LN1897/PF259243
-Hannibal-
2016-01-29 3:18 AM
However, the wording of the OP's request suggests such a project might be a little over his head at the moment.
I would suggest to start with something simpler first, to avoid frustration.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.