2015-09-18 3:46 AM
I accidentaly did something bad to my flash memory on stm32f3. I tried to disable the write protection to the whole flash but in the result now I have the whole flash write protected and cant debug any program ( I checked it using st-link utility). Is there anyway to fix it?
Regards2015-09-18 5:21 AM
Hi oziom.dominik,
If you are at Level2, unfortunately nothing can be done: Memory read protection Level 2 is an irreversible operation. When Level 2 is activated,the level of protection cannot be decreased to Level 0 or Level 1.If you are in level 1: you can use STM32 ST-LINK Utility: Target > Option Bytes to modify protection -Syrine –2015-09-18 5:46 AM
Thanks for fast answer. Good for me it wasn't a level 2. Changing Data 0(H) value to 0x00 in option bytes settings solved the problem.
Regards Dominik O.2015-09-18 5:55 AM
It is good to hear that it was solved.
-Syrine –We’re moving the ST Community to a new platform to give you a better and more reliable community experience.