2013-02-07 11:06 PM
Hello.
I have a question concerning processor 96bit UID. I understand that this number is ST unique number and I would like to use it as a board identification in production. But the number is farly long for expressing in text form. So I would like to short it to be unique relative for certain chip. I see that DFU boatloader uses a shorter serial number similar to UID and it differs among similar chips. Would anybody know the number meaning or a mask reducing the number to demanded purpose? Thank you. #id-unique-meaning-shortening2013-09-25 3:25 AM
> duplicated UID.
Well that id is good for shyte.. Is this something known to happen? At least from the STM32F1 manual, there is very strong emphasis on uniqueness. ''The 96-bit unique device identifier provides a reference number which is unique for anydevice and in any context. These bits can never be altered by the user. The 96-bit unique device identifier can also be read in single bytes/half-words/words in
different ways and then be concatenated using a custom algorithm.''
2013-09-25 6:42 AM
> duplicated UID.
Well that id is good for shyte.. Is this something known to happen?
At least from the STM32F1 manual, there is very strong emphasis on uniqueness.
''The 96-bit unique device identifier provides a reference number which is unique for any device and in any context. These bits can never be altered by the user.
The 96-bit unique device identifier can also be read in single bytes/half-words/words in different ways and then be concatenated using a custom algorithm.'' It doesn't preclude you or someone else fouling up the implementation, and I'm saying that your test procedures should have enough integrity to catch such things.[DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Unique%20Device%20ID%20not%20unique%21&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&TopicsView=https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/AllItems.aspx¤tviews=84]https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fcortex_mx_stm32%2fUnique%20Device%20ID%20not%20unique!&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&TopicsView=https%3A%2F%2Fmy.st.com%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2Fcortex_mx_stm32%2FAllItems.aspx¤tviews=84
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.