STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 USB library - CDC_Send_DATA()

Posted on September 25, 2013 at 20:09Hi all,Currently I'm working on an application that will call CDC_Send_DATA() periodically. However, if I call it too often, some packets will be missing somewhere in the middle.  Does anyone know the reason?  Th...

bypass/electrical short STM32F0 Discovery

Posted on September 25, 2013 at 14:17Hi,I'm programming the STM32F0Discovery. Well, I made a short circuit between the 5V pin and the GND pin while measuring. Now I can't programm the board anymore. The COM-LED (LD2) is turned off all the time and I...

Dead time accessed when?

Posted on September 25, 2013 at 09:07HiI need to be able to adjust the dead time of one of the advanced timers in an F4 during execution.I can easily write to the BDTR register but it seems a bit dangerous to do so without knowing when the timer wil...

marbel by Associate II
  • 875 Views
  • 1 replies
  • 0 kudos

Unique 96bit ID meaning and its shortening

Posted on February 08, 2013 at 08:06Hello. I have a question concerning processor 96bit UID. I understand that this number is ST unique number and I would like to use it as a board identification in production. But the number is farly long for expre...

kinovicf by Associate II
  • 8591 Views
  • 11 replies
  • 0 kudos

do you need to explictly set SCB->CCR |= SCB_CCR_STKALIGN;

Posted on September 25, 2013 at 14:42''Immediately after stacking, the stack pointer indicates the lowest address in the stack frame. Unless stack alignment is disabled, the stack frame is aligned to a double-word address. If the STKALIGN bit of the...

denis by Associate II
  • 1103 Views
  • 0 replies
  • 0 kudos

STM32L162 eval kit?

Posted on September 25, 2013 at 03:11Hi,May I know is there any evaluation kit for STM32L162? I know there is kit for L152.

STM32F4 Bootloader pins connection problem (AN2606)?

Posted on September 24, 2013 at 09:34Hello. I'm using STM32F405RG. In my application we plan to use bootloader on USART1 for firmware programming. In AN2606 page 74 is written, that the rest of bootloader channels (USART3, CAN and OTG) inputs must b...

mudrovc2 by Associate II
  • 1184 Views
  • 1 replies
  • 0 kudos

smt32f4 - arm-none-eabi makefile

Posted on September 23, 2013 at 11:19Hi all, I'm trying to write a makefile for arm-none-eabi toolchain (Menthor arm-2013.05-23-arm-none-eabi-i686-pc-linux-gnu). The file compile all project without error but I have several questions about this proc...

sarraciro by Associate II
  • 3212 Views
  • 6 replies
  • 0 kudos

A word of warning... (and a request for explaination)

Posted on September 23, 2013 at 21:45So, I'm currently working on a side project at home for a LED driver/controller board. In the process of this, I've decided to use a STM8 for some additional A/D and to offload the averaging. I got the eval board...

dciliske by Associate
  • 1626 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.