2024-11-19 2:46 AM
Hi,
We notice the startup time from power up can be affected by setting one GPIOB pin to input. The startup time here refers to the time from SystemInit() until main(). Basically it contains scatterload and __rt_entry to my understanding.
Specifically, the sample code below, built with ARM Compiler 6.16 Tool, would demonstrate that
#define MEASURE_PIN 5
int main(void)
{
IO_SET_PIN(GPIOA, MEASURE_PIN, 1);
// Enable IWDG
IWDG->KR = 0xCCCC;
// Enable write access
IWDG->KR = 0x5555;
// Set prescaler
IWDG->PR = 0;
// Set reload
IWDG->RLR = 1;
// Wait for the registers reload
while (IWDG->SR)
{
}
// refresh the watchdog.
IWDG->KR = 0xAAAA;
while(1);
return 0;
}
void SystemInit(void)
{
// enable GPIOA clock
RCC->IOPENR |= RCC_IOPENR_GPIOAEN | RCC_IOPENR_GPIOBEN;
// set GPIOA pin5 to output
IO_SET_PIN_DIR(GPIOA, MEASURE_PIN, 1);
// set GPIOA pin5 to low
IO_SET_PIN(GPIOA, MEASURE_PIN, 0);
// Set GPIOB pin7 to input
// GPIOB->MODER &= 0xffff3fff;
} Basically GPIOA pin 5 is toggled to low and high for the time between SystemInit() and main() to be measured.
main() also has IWDG setup and ends with a while loop so that IWDG reset happens periodically since power up.
On the oscilloscope it looks like the screenshots below.
Respectively from the screenshots, it can be observed that the 1st startup(power up) takes 254 μs while the 2nd startup (IWDG reset) takes 132 μs.
Now if uncommenting this line GPIOB->MODER &= 0xffff3fff; and redo the measurement, we get the results below.
We can see that having the GPIOB pin 7 set to input reduces the startup time from 254 μs to 132 μs and the rest startup remains taking the same time.
Could you please confirm the following:
Just in case, this is how Reset_Handler looks like in our startup file. It is basically without any customization.
; Reset handler routine
Reset_Handler PROC
EXPORT Reset_Handler [WEAK]
IMPORT __main
IMPORT SystemInit
LDR R0, =SystemInit
BLX R0
LDR R0, =__main
BX R0
ENDPAnta
Solved! Go to Solution.
2024-12-10 5:42 AM
> Push on the stack? Does SystemInit even need stack?
It's a normal C function.
While in this particular case the registers wouldn't need to be preserved, there's no guarantee that that is the case generally.
> Would marking the function as _Noreturn or __attribute__((noreturn)) help?
It's a normal C function which does return.
> I think we need to ask the engineers who designed the chip
Developers with the required knowledge are highly unlikely to turn up here. The OP may ask ST directly, but I wouldn't hold my breath.
> They should know what conditions trigger this behavior and perhaps how to avoid it.
Most probably power-on reset triggers it. Maybe RAM_PARITY_CHECK option bit is involved. I don't have a C0 to try and also I am not interested in this that much; OP may try to check this.
You can also try to write your program so that it won't touch RAM for quite some time (e.g. initialize clocks, peripherals meantime), if you really need every microsecond of powerup startup latency. Note, that t RSTTEMPO = typ.270us max. 500us.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.