2023-07-12 5:24 AM
Hi all,
i am using stm32f3 discovery EV kit, i am using stand by mode for deep sleep, but it is not wake up from sleep mode.
i configured sys_wkup1 (PA0) and it is connected push button.i am re intialize i/o port and toggling one led after wake up from sleep. when i pressed the button nothing is occur. when i connected mutli meter it is showing 4 uamps when button pressed it is increased 10uamps, but when releasing button it is 4uamps. when i debugging it is gone to Error_Handler function. i am sharing firmware below.
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
//MX_TIM2_Init();
// MX_ADC1_Init();
/* USER CODE BEGIN 2 */
HAL_GPIO_TogglePin(LD3_GPIO_Port, LD3_Pin);
HAL_Delay(2000);
HAL_GPIO_TogglePin(LD3_GPIO_Port, LD3_Pin);
HAL_Delay(2000);
HAL_PWR_EnableWakeUpPin( GPIO_PIN_0);
HAL_PWR_EnableWakeUpPin( GPIO_MODE_IT_RISING);
HAL_SuspendTick();
__HAL_RCC_PWR_CLK_ENABLE();
HAL_PWR_EnterSTANDBYMode();
HAL_ResumeTick(); // Resume Tick interrupt if disabled prior to sleep mode entry
MX_TIM2_Init();
MX_GPIO_Init();
while (1)
{
/* USER CODE END WHILE */
HAL_GPIO_TogglePin(LD3_GPIO_Port, LD3_Pin);
HAL_Delay(2000);
/* USER CODE BEGIN 3 */
}
please give any solutions
regards,
nraj
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.