2024-07-09 7:28 AM - edited 2024-07-09 10:00 PM
Hello,
I am trying to send the message from my USB-CAN Analyzer to my board STM32F407 discovery board, but I am unable to do that.
HAL_CAN_GetRxMessage(&hcan1, CAN_RX_FIFO0, &rx_header, rx_data);
// Process received message
handleReceivedMessage(&rx_header, rx_data);
This is my function to read message.
void handleReceivedMessage(CAN_RxHeaderTypeDef *rx_header, uint8_t *rx_data)
{
// Your custom handling of received message
// Example: LED blinking based on received data
HAL_GPIO_TogglePin(GPIOB, GPIO_PIN_12); // Toggle LED
}
This is my handlereceivedMessage function.
Below is my message which I am sending from USB-CAN Analyzer.
Best Regards
Rohit Kumar
Solved! Go to Solution.
2024-07-10 6:01 AM
In that case I suspect the following issues:
1- A HW issue: check your wiring, the power supply of the transceiver , your transceiver connections, termination resistors. In that case you need to provide schematics of your board.
2- Bit timing issue: are you sure you have the same bitrate config as for your CAN analyzer?
3- The clock source: are you sing HSE and a crystal? if not you can face issue with CAN communication in normal mode.
You need also to share your project as requested previously.
2024-07-09 7:42 AM - edited 2024-07-09 7:47 AM
Hello,
In this previous thread I recommended you to review on how to post a thread on this community: https://community.st.com/t5/community-guidelines/how-to-write-your-question-to-maximize-your-chances-to-find-a/ta-p/575228
Could you please review it again and edit your post accordingly?
Thank you for your understanding
2024-07-10 12:08 AM - edited 2024-07-10 12:25 AM
Hello,
Hello,
I am trying to send the message from my USB-CAN Analyzer to my board STM32F407 discovery board, but I am unable to do that.
while (1)
{
CAN_RxHeaderTypeDef rxHeader;
uint8_t rx_data[8];
HAL_CAN_GetRxMessage(&hcan1, CAN_RX_FIFO0, &rxHeader, rx_data);
{
// Process received message
handleReceivedMessage(&rxHeader, rx_data);
}
}
This is my function to read message.
void handleReceivedMessage(CAN_RxHeaderTypeDef *rx_header, uint8_t *rx_data)
{
// Your custom handling of received message
// Example: LED blinking based on received data
HAL_GPIO_TogglePin(GPIOB, GPIO_PIN_12); // Toggle LED
}
This is my handlereceivedMessage function.
I have configured the interrupt too.
/*Enable CAN RX FIFO Interrupt in NVIC*/
HAL_NVIC_SetPriority(CAN1_RX0_IRQn, 0, 0); // Set priority
HAL_NVIC_EnableIRQ(CAN1_RX0_IRQn); // Enable interrupt
Below is my Can bit timing and filter configuration.
static void MX_CAN1_Init(void)
{
/* USER CODE END CAN1_Init 1 */
hcan1.Instance = CAN1;
hcan1.Init.Prescaler = 4;
hcan1.Init.Mode = CAN_MODE_NORMAL;
hcan1.Init.SyncJumpWidth = CAN_SJW_1TQ;
hcan1.Init.TimeSeg1 = CAN_BS1_12TQ;
hcan1.Init.TimeSeg2 = CAN_BS2_3TQ;
hcan1.Init.TimeTriggeredMode = DISABLE;
hcan1.Init.AutoBusOff = DISABLE;
hcan1.Init.AutoWakeUp = DISABLE;
hcan1.Init.AutoRetransmission = DISABLE;
hcan1.Init.ReceiveFifoLocked = DISABLE;
hcan1.Init.TransmitFifoPriority = DISABLE;
if (HAL_CAN_Init(&hcan1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN CAN1_Init 2 */
CAN_FilterTypeDef can_filter;
can_filter.FilterIdHigh = 0x0000;
can_filter.FilterIdLow = 0x0000;
can_filter.FilterMaskIdHigh = 0x0000;
can_filter.FilterMaskIdLow = 0x0000;
can_filter.FilterFIFOAssignment = CAN_FILTER_FIFO0;
can_filter.FilterBank = 1;
can_filter.FilterMode = CAN_FILTERMODE_IDMASK;
can_filter.FilterScale = CAN_FILTERSCALE_32BIT;
can_filter.FilterActivation = CAN_FILTER_ENABLE;
can_filter.SlaveStartFilterBank = 2;
if (HAL_CAN_ConfigFilter(&hcan1, &can_filter) != HAL_OK)
{
Error_Handler();
}
}
I review it again and edit accordingly. The problem in the above query I am facing is the form error. I have my bit timing set to the 75% point. SJW=1, BS1=14, BS2= 5, 500,000baud. Could you please check and recommend me some accurate values for bit timings so that i can overcome this form error.
2024-07-10 1:16 AM - edited 2024-07-10 1:20 AM
Hello,
You activated the CAN interrupt :
HAL_NVIC_SetPriority(CAN1_RX0_IRQn, 0, 0); // Set priority
HAL_NVIC_EnableIRQ(CAN1_RX0_IRQn); // Enable interrupt
but you didn't use it and in the while loop you didn't check if a message has been received or not. This is not the correct implementation.
I suggest you to review the example provided in STM32CubeF4 in this path under https://github.com/STMicroelectronics/STM32CubeF4/tree/master/Projects/STM324xG_EVAL/Examples/CAN/CAN_Networking.
Also could you please attach your project (including the ioc file if there is one)?
2024-07-10 3:47 AM
Hello,
I am getting form error in CAN_ESR. According to my above configurations correct my bit timing configurations.
Best regards
Rohit Kumar
2024-07-10 4:58 AM
I think you accidently marked my answer as solution. I unmarked it then.
Need to check you bitrate config + the clock source config: need to have the same CAN bitrate as your CAN analyzer + If you are using HSI you need to change it to HSE with an external crystal.
But as a starting point use Loopback mode to at least validate your send/receive operations. If in Loopback mode doesn't work, it doesn't work also for Normal mode.
2024-07-10 5:46 AM
Hello,
My configuration works for the loopback mode, but it doesn't work for the normal mode.
B.R
Rohit Kumar
2024-07-10 6:01 AM
In that case I suspect the following issues:
1- A HW issue: check your wiring, the power supply of the transceiver , your transceiver connections, termination resistors. In that case you need to provide schematics of your board.
2- Bit timing issue: are you sure you have the same bitrate config as for your CAN analyzer?
3- The clock source: are you sing HSE and a crystal? if not you can face issue with CAN communication in normal mode.
You need also to share your project as requested previously.
2024-07-11 12:08 AM
Hello,
Can you suggest me how to implement HAL_CAN_GetRxFifoFillLevel for the reception of messages.
Explain it with example for just only reception.
B.R
Rohit Kumar
2024-07-11 1:03 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.