2021-11-28 7:03 AM
Hello ,
I will power a stm32 pcb with battery so the vdd voltage will drop
So i need to read this VDD to make a conversion of external temp sensor from 0->4096 to a voltage
Voltage temp=(VDD*adc_value/4096)
But my chip only have one ADC and i'm unable to have correct value when i try to read VREFINT and a other channel
------------------------------------------------------
TERMINAL VALUE:
VREFINT=3.8V (chip will die )
PA6=1.16V (connected to GND)
-------------------------------------------------------
CODE FOR DMA :
HAL_ADC_Start_DMA(&hadc1,value,2);
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
char MSG[100];
float Vdd;
Vdd = 3300 * (*VREFINT_CAL_ADDR)/ value[1];
Vdd=Vdd/1000;
sprintf(MSG,"La tension est de : %f V\r\n",Vdd);
HAL_UART_Transmit(&huart2,MSG,sizeof(MSG),1000);
char MSG1[100];
float PA7;
PA7=((Vdd*value[0])/4095.0f);
sprintf(MSG1,"La tension de PA6 est de : %f V\r\n",PA7);
HAL_UART_Transmit(&huart2,MSG1,sizeof(MSG1),1000);
/* USER CODE BEGIN 3 */
}
---------------------------------------------------------------------------------------
CODE FOR CHANGING THE CHANNEL WHEN WE WANT TO READ IT
void ADC_Select_CH12 (void)
{
ADC_ChannelConfTypeDef sConfig = {0};
/** Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time.
*/
sConfig.Channel = ADC_CHANNEL_12;
sConfig.Rank = 1;
sConfig.SamplingTime = ADC_SAMPLETIME_247CYCLES_5;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
}
void ADC_Select_VREF (void)
{
ADC_ChannelConfTypeDef sConfig = {0};
/** Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time.
*/
sConfig.Channel = ADC_CHANNEL_VREFINT;
sConfig.Rank = 1;
sConfig.SamplingTime = ADC_SAMPLETIME_247CYCLES_5;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
}
while (1)
{
/* USER CODE END WHILE */
uint16_t ADC_VAL[1000];
ADC_Select_VREF();
HAL_ADC_Start(&hadc1);
HAL_ADC_PollForConversion(&hadc1, 1000);
ADC_VAL[0] = HAL_ADC_GetValue(&hadc1);
HAL_ADC_Stop(&hadc1);
char MSG[100];
float Vdd;
Vdd = 3300 * (*VREFINT_CAL_ADDR)/ ADC_VAL[0];
Vdd=Vdd/1000;
sprintf(MSG,"La tension est de : %f V\r\n",Vdd);
HAL_UART_Transmit(&huart2,MSG,sizeof(MSG),1000);
HAL_Delay(100);
ADC_Select_CH12();
HAL_ADC_Start(&hadc1);
HAL_ADC_PollForConversion(&hadc1, 1000);
char MSG1[100];
ADC_VAL[1] = HAL_ADC_GetValue(&hadc1);
HAL_ADC_Stop(&hadc1);
float PA6;
PA7=((Vdd*ADC_VAL[1])/4095.0f);
sprintf(MSG1,"La tension de PA6 est de : %f V\r\n",PA7);
HAL_UART_Transmit(&huart2,MSG1,sizeof(MSG1),1000);
/* USER CODE BEGIN 3 */
}
------------------------------------------------------------------
So where i'm wrong and do you have some ideas to correct this
Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.