2024-05-15 11:48 PM - edited 2024-05-15 11:49 PM
Hi all,
i'm working with a STM32F469i-discovery board trying to read the external signal at 32kHz coming from an RTC module. The oscillating signal voltage is a CMOS type. I'm using TIM2_ETR input located on pin PA15 configured as follow. I'm not able to read any pulse on the pin and every time that I run the system the oscillator voltage fall to 0.3V instead of the 2.5V that I can measure when the system is not running.
I test the oscillator signal on Arduino board and I can read the right frequency just connectin the oscillator output to Arduino pin8. Thanks for the support.
2024-05-16 7:36 AM
Ok, what you see on pin with scope ? clk signal ok ?
+
set counter period to some lower value for test, maybe 2000 .
2024-05-16 9:00 AM - edited 2024-05-19 2:26 AM
In particular CCER=1 means, that CH1 is enabled; and as in CCMR1 it is set to Output compare, given pin turns to output (TIM2_CH1 is shared with TIM2_ETR on PA15).
I don't use Cube/CubeMX so can't tell how can you avoid this using Cube/CubeMX. It may be a bug in Cube/CubeMX.
I generally recommend you to use register-based programming instead, but some here find that an extereme approach.
JW
PS. Maybe similar https://community.st.com/t5/stm32-mcus-boards-and-hardware/tim2-tim3-tim4-ert-mode-on-nucleo-h743zi2/td-p/676201
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.