2015-05-01 2:23 AM
Hello,
I�m quit new to STs micro controllers and openocd. I want to use the STM32L152RE on a Nucleo board. I�ve installed the head version of openocd to get support for this board. I start openocd with following parameters:
openocd -f board/st_nucleo_l1.cfg
My .gdbinit file looks like this:
target remote localhost:3333
monitor reset symbol /Users/todi/ebtks/build/source/ebtks.elfWhen starting gdb, it looks like that every time the PC of the CPU is at 0x08000242:
> arm-none-eabi-gdb
�
0x08000242 in ?? ()
Unable to match requested speed 300 kHz, using 240 kHz Unable to match requested speed 300 kHz, using 240 kHz adapter speed: 240 kHz Breakpoint 1 at 0x800019c: file /Users/todi/ebtks/source/main.cpp, line 26.According to the elf-file this is within the Reset_Handler:0800023c <FillZerobss>:
800023c: 2300 movs r3, &sharp0 800023e: f842 3b04 str.w r3, [r2], &sharp4 08000242 <LoopFillZerobss>: 8000242: 4b09 ldr r3, [pc, &sharp36] ; (8000268 <LoopFillZerobss+0x26>) 8000244: 429a cmp r2, r3 8000246: f4ff aff9 bcc.w 800023c <FillZerobss> 800024a: f7ff ffb3 bl 80001b4 <SystemInit>when ever I try to debug the CPU I do not get to main() but end up with a PC of 0x08000242
(gdb) monitor reset
Unable to match requested speed 300 kHz, using 240 kHz Unable to match requested speed 300 kHz, using 240 kHz adapter speed: 240 kHz (gdb) s Single stepping until exit from function LoopFillZerobss, which has no line number information. Note: automatically using hardware breakpoints for read-only addresses. WARNING! The target is already running. All changes GDB did to registers will be discarded! Waiting for target to halt. ^C Program received signal SIGINT, Interrupt. 0x08000242 in LoopFillZerobss ()Is the warning a hint that resetting the CPU isn�t working as expected? Are there any addition setting I would have to set with openocd or gdb?
thanks in advance for any help or pointers,
Torsten
#openocd-gdb-stm32l12015-05-05 8:46 AM
I’ve fixed the problem with a tipp from the openocd mailing list. There is a different method to connect the gdb to the openocd server:
target extended-remote localhost:3333
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.