2015-04-28 3:51 PM
After adding the CRC peripheral for an STM32F415 project...
CubeMX bug: stm32f4xx_hal_crc.c is not included in IAR project. The main.c code does have the code to create a handle and all the init code is brought in. But stm32f4xx_hal_crc.c is not in the project's Driver folders, either CMSIS or the HAL drivers folder. The compiler thus errors, with HAL_CRC_Init not found. If I manually add stm32f4xx_hal_crc.c to the project, no more errors. So CubeMX forgot to include the .c but did everything else OK.2015-04-29 5:43 AM
Sounded familiar, well similar at least
2015-04-30 9:11 PM
That bug reported for release 4.6 did NOT get fixed in 4.7. What is the configuration management and bug tracking system used by ST for its tools?
2015-05-01 3:57 AM
That bug reported for release 4.6 did NOT get fixed in 4.7. What is the configuration management and bug tracking system used by ST for its tools?
And what is the test coverage for those CubeMX releases ? It would probably be helpful to publish some kind of test matrix: which example was tested with wich hardware (board), and which CubeMX version, and perhaps including test results. Not to speak of tests with peripheral combinations... As an hobbyist in the MCU world, I can easily shun such stuff, and hold on to working tools/libraries. I have not yet regretted the decision to stick to the SPL...
2015-05-05 7:05 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.