2023-12-19 8:37 PM
Hello Experts,
I designed my custom board with reference to AN5419 application note (Getting started with STM32H723/733, STM32H725/735 and STM32H730 Value Line hardware development). but it doesn't work.
When i apply to power to the board and connect it to ST-Link utility, Program is displayed "can not connect to target".
I'm a newbie about circuit design. so i referenced the application notes but I am not sure if it's designed properly.
I simply want to use GPIO port and communications.
Please let me know what i can check.
Sincerely,
SH.
Solved! Go to Solution.
2023-12-19 9:09 PM - edited 2023-12-19 9:10 PM
Quite a few things not following the application note:
I feel like none of the above issues is the root cause though. Could be wrong.
As with any chip that is unresponsive:
> ST-Link utility
Has been deprecated for many years and doesn't work with H7 family.
2023-12-19 8:58 PM
The ST-LINK Utilities are too old. You need to be using STM32 Cube Programmer.
Check power and ground connection to ST-LINK and SWDIO/SWCLK are the right way around.
2023-12-19 9:06 PM
Thank you for your quick response.
However, I also tried to connect to STM32CubeIDE but it doesn't connect.
Below is the contents of the console.
STMicroelectronics ST-LINK GDB server. Version 7.5.0
Copyright (c) 2023, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Target no device found
Error in initializing ST-LINK device.
Reason: No device found on target.
2023-12-19 9:09 PM - edited 2023-12-19 9:10 PM
Quite a few things not following the application note:
I feel like none of the above issues is the root cause though. Could be wrong.
As with any chip that is unresponsive:
> ST-Link utility
Has been deprecated for many years and doesn't work with H7 family.
2023-12-20 1:15 AM - edited 2023-12-20 1:17 AM
Hello, i tried what you propsed. unfortunately, but, it doesn't still work.
I resoldered VCAP with the attached file... is that correct?
VDD and VDDA voltage is 3.29V. (using Digital multimeter)
VCAP voltage is 0.9mV (VCAP1, 2, 3)
and i tried using STM32CubeProgrammer.
I appriciated your help. but is there any other checklist i can try it?
2023-12-20 6:08 AM
> VCAP voltage is 0.9mV (VCAP1, 2, 3)
This is an issue that will prevent booting. Something isn't right with your hardware. Your change looks good, however.
Perhaps there are workmanship issues. Perhaps bad solder joints or solder bridges.
> I appriciated your help. but is there any other checklist i can try it?
Perhaps show a high resolution photo of the board.
Does STM32CubeProgrammer recognize your programmer? Does it show target voltage correctly?
2023-12-20 10:47 PM - edited 2023-12-21 4:00 AM
Hello TDK,
VCAP capacitors should be 2x2.2 uF. VCAP pins should be tied.
> I tried again with another board. Fortunately, I confirmed that it is connected to STM32CubeProgrammer. Probably, I think i made a mistake while resoldering.
Thank you so much for your advice. but I should be more careful next time..
Sincerely
SH.
2023-12-21 7:16 PM
In addition to what TDK noted, the R115 is also unnecessary and will cause HSE issues. And what for exactly is the D11 there?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.