2025-05-18 6:32 AM
Dear together,
For the past dew days Im stuck kwith UART communication with DMA.
To start with, I am implementing TX now. Later I will implement RX. I have managed for TX to work without interrupt. As per my application, I need Interrupt to inform the micro controller when transmission is completed.
But when I enabled the DMA_CCR_TCIE bit in DMA1_Channel2->CCR, micro controller hangs. For your information, I have provided my code here.
This is the function to Initialize DMA
void Init_DMA(void)
{
// Enable clock for DMA1 peripheral by setting the DMA1EN bit in RCC AHBENR register
RCC->AHBENR |= RCC_AHBENR_DMA1EN;
// Enable DMA1_Channel2_3 interrupt in NVIC
NVIC_EnableIRQ(DMA1_Channel2_3_IRQn);
// Set priority for DMA1_Channel2_3 interrupt (Preemption = 0, Sub = 0)
NVIC_SetPriority(DMA1_Channel2_3_IRQn, 0);
}
This is the function to Initialize UART1
void Init_UART1(void)
{
// 1. Enable clocks for GPIOB, USART1, and DMA1
RCC->AHBENR |= RCC_AHBENR_GPIOBEN;
RCC->APB2ENR |= RCC_APB2ENR_USART1EN;
// 2. Configure PB5 as DE output (push-pull, high speed)
GPIOB->MODER &= ~(3 << (5 * 2));
GPIOB->MODER |= (1 << (5 * 2)); // Output mode
GPIOB->OTYPER &= ~(1 << 5); // Push-pull
GPIOB->OSPEEDR |= (3 << (5 * 2)); // High speed
GPIOB->PUPDR &= ~(3 << (5 * 2)); // No pull
GPIOB->ODR &= ~(1 << 5); // Set DE LOW (receive mode)
// 3. Configure PB6 as USART1_TX (AF0)
GPIOB->MODER &= ~(3 << (6 * 2));
GPIOB->MODER |= (2 << (6 * 2)); // Alternate function
GPIOB->OTYPER &= ~(1 << 6); // Push-pull
GPIOB->OSPEEDR |= (3 << (6 * 2)); // High speed
GPIOB->PUPDR &= ~(3 << (6 * 2));
GPIOB->PUPDR |= (1 << (6 * 2)); // Pull-up
GPIOB->AFR[0] &= ~(0xF << (6 * 4));
GPIOB->AFR[0] |= (0x0 << (6 * 4)); // AF0 = USART1
// Reset USART1
USART1->CR1 = 0;
USART1->CR2 = 0;
USART1->CR3 = 0;
USART1->BRR = Set_USART1_BRR; // Set baud rate
switch (Set_Parity)
{
case 0: // 8N2 (No parity, 2 stop bits)
USART1->CR1 &= ~USART_CR1_PCE;
USART1->CR1 &= ~USART_CR1_M;
USART1->CR2 &= ~USART_CR2_STOP;
USART1->CR2 |= USART_CR2_STOP_1 | USART_CR2_STOP_0; // 2 stop bits
break;
case 1: // 8E1 (Even parity, 1 stop bit)
USART1->CR1 |= USART_CR1_PCE;
USART1->CR1 &= ~USART_CR1_PS;
USART1->CR1 |= USART_CR1_M;
USART1->CR2 &= ~USART_CR2_STOP; // 1 stop bit
break;
case 2: // 8O1 (Odd parity, 1 stop bit)
USART1->CR1 |= USART_CR1_PCE;
USART1->CR1 |= USART_CR1_PS;
USART1->CR1 |= USART_CR1_M;
USART1->CR2 &= ~USART_CR2_STOP; // 1 stop bit
break;
}
// 1 stop bit: CR2 STOP[1:0] = 00 (default, so we can skip)
// Enable transmitter and receiver
USART1->CR1 |= USART_CR1_TE | USART_CR1_RE;
// Enable USART
USART1->CR1 |= USART_CR1_UE;
}
This is the function used to transfet the data throgh DMA
void MB_Frame_Transmit(volatile uint8_t *data, uint16_t len)
{
uart_tx_busy = 1;
SET_DE; // Enable RS485 Transmit mode
// Disable DMA channel before reconfiguring
DMA1_Channel2->CCR &= ~DMA_CCR_EN;
// Clear DMA interrupt flags for Channel 2
DMA1->IFCR = DMA_IFCR_CTCIF2 | DMA_IFCR_CTEIF2;
// Configure DMA Channel 2 for USART1_TX
DMA1_Channel2->CNDTR = len;
DMA1_Channel2->CPAR = (uint32_t)&USART1->TDR;
DMA1_Channel2->CMAR = (uint32_t)data;
// Reconfigure DMA Channel 2
DMA1_Channel2->CCR =
DMA_CCR_MINC | // Memory increment
DMA_CCR_DIR | // Read from memory (TX)
/*DMA_CCR_TCIE | // Enable transfer complete interrupt*/
DMA_CCR_PL_1; // High priority (optional)
// Enable USART1 TX DMA mode
USART1->CR3 |= USART_CR3_DMAT;
// Enable DMA Channel 2
DMA1_Channel2->CCR |= DMA_CCR_EN;
}
This is the ISR
void DMA1_Channel2_3_IRQHandler(void)
{
// Check Transfer Complete interrupt for Channel 2
if (DMA1->ISR & DMA_ISR_TCIF2)
{
// Clear transfer complete flag
DMA1->IFCR = DMA_IFCR_CTCIF2;
// Disable DMA Channel 2 and USART DMA mode
DMA1_Channel2->CCR &= ~DMA_CCR_EN;
USART1->CR3 &= ~USART_CR3_DMAT;
uart_tx_busy = 0;
CLEAR_DE; // Set RS485 to Receive mode
}
// Optional: handle transfer error (TEIF2)
if (DMA1->ISR & DMA_ISR_TEIF2)
{
DMA1->IFCR = DMA_IFCR_CTEIF2;
// You can set an error flag or retry here
Switch_Reset_LED_ON;
}
}
I call the DMA1_Channel2_3_IRQHandler() function from main once in 600 mS. With this loop delay. I will not re initiate the DMA transfer before previous transfer is completed. delay_ms() is the blocking function implemented by timer 14.
Now the interesting part: If I disable the TCIE bit inise the MB_Frame_Transmit() function, DMA transfer happens perfectly once in 600ms. I probe this in my oscilloscope and confirm.
But if I enable TCIE, transmission happens only for first time when micro controller is restarted. Then it hangs.
Few more observations. This is my main function
int main(void)
{
Config_System_Clock();
Init_GPIOs();
Init_DMA();
Init_UART1();
Init_Tim14_1ms();
__enable_irq();
for (uint8_t i = 0; i < 10; ++i) { TX_Array[i] = i; }
//UART1_Transmit_DMA(TX_Array, 10);
SET_DE;
//Switch_Reset_LED_ON;
while(1)
{
MB_Frame_Transmit(TX_Array, 10);
Switch_Status_LED_ON; delay_ms(300);
Switch_Status_LED_OFF; delay_ms(300);
}
}When the TCIE is enabled, the status LED is turned ON then not turned OFF. When means just for one time Switch_Statsu_LED_ON funtion is executed once then nothing further. Also the Reset LED placed insde Error handler is not turned, ON. which means means that part of ISR is also not executed.
Please let me know, what is the issue in my code.
Thank you, Anesh S.
Solved! Go to Solution.
2025-05-20 12:05 PM
Cool, thank you for the information.
I am also planning to use IDLE interrupt to start a timer in One Pulse Mode to run 3.5 times of 11 bits (A byte as per Modbus protocol). So if the receiver is silent for 3.5 times of a byte (around 4 ms for 9600 Baudrate), then I will decide frame is completed and start processing.
I have already implemented complete Modbus protocol (All standard function codes) with TX (TCIE) and RX (RXNE) ISRs. things are working fine. Though controller not much loaded with interrupts, I want to further reduce number of interrupts and make controller available for some other functions (which are not yet planned :))
Let me try RX with DMA too, and trouble experts like you by starting another post :)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.