2025-05-18 6:32 AM
Dear together,
For the past dew days Im stuck kwith UART communication with DMA.
To start with, I am implementing TX now. Later I will implement RX. I have managed for TX to work without interrupt. As per my application, I need Interrupt to inform the micro controller when transmission is completed.
But when I enabled the DMA_CCR_TCIE bit in DMA1_Channel2->CCR, micro controller hangs. For your information, I have provided my code here.
This is the function to Initialize DMA
void Init_DMA(void)
{
// Enable clock for DMA1 peripheral by setting the DMA1EN bit in RCC AHBENR register
RCC->AHBENR |= RCC_AHBENR_DMA1EN;
// Enable DMA1_Channel2_3 interrupt in NVIC
NVIC_EnableIRQ(DMA1_Channel2_3_IRQn);
// Set priority for DMA1_Channel2_3 interrupt (Preemption = 0, Sub = 0)
NVIC_SetPriority(DMA1_Channel2_3_IRQn, 0);
}
This is the function to Initialize UART1
void Init_UART1(void)
{
// 1. Enable clocks for GPIOB, USART1, and DMA1
RCC->AHBENR |= RCC_AHBENR_GPIOBEN;
RCC->APB2ENR |= RCC_APB2ENR_USART1EN;
// 2. Configure PB5 as DE output (push-pull, high speed)
GPIOB->MODER &= ~(3 << (5 * 2));
GPIOB->MODER |= (1 << (5 * 2)); // Output mode
GPIOB->OTYPER &= ~(1 << 5); // Push-pull
GPIOB->OSPEEDR |= (3 << (5 * 2)); // High speed
GPIOB->PUPDR &= ~(3 << (5 * 2)); // No pull
GPIOB->ODR &= ~(1 << 5); // Set DE LOW (receive mode)
// 3. Configure PB6 as USART1_TX (AF0)
GPIOB->MODER &= ~(3 << (6 * 2));
GPIOB->MODER |= (2 << (6 * 2)); // Alternate function
GPIOB->OTYPER &= ~(1 << 6); // Push-pull
GPIOB->OSPEEDR |= (3 << (6 * 2)); // High speed
GPIOB->PUPDR &= ~(3 << (6 * 2));
GPIOB->PUPDR |= (1 << (6 * 2)); // Pull-up
GPIOB->AFR[0] &= ~(0xF << (6 * 4));
GPIOB->AFR[0] |= (0x0 << (6 * 4)); // AF0 = USART1
// Reset USART1
USART1->CR1 = 0;
USART1->CR2 = 0;
USART1->CR3 = 0;
USART1->BRR = Set_USART1_BRR; // Set baud rate
switch (Set_Parity)
{
case 0: // 8N2 (No parity, 2 stop bits)
USART1->CR1 &= ~USART_CR1_PCE;
USART1->CR1 &= ~USART_CR1_M;
USART1->CR2 &= ~USART_CR2_STOP;
USART1->CR2 |= USART_CR2_STOP_1 | USART_CR2_STOP_0; // 2 stop bits
break;
case 1: // 8E1 (Even parity, 1 stop bit)
USART1->CR1 |= USART_CR1_PCE;
USART1->CR1 &= ~USART_CR1_PS;
USART1->CR1 |= USART_CR1_M;
USART1->CR2 &= ~USART_CR2_STOP; // 1 stop bit
break;
case 2: // 8O1 (Odd parity, 1 stop bit)
USART1->CR1 |= USART_CR1_PCE;
USART1->CR1 |= USART_CR1_PS;
USART1->CR1 |= USART_CR1_M;
USART1->CR2 &= ~USART_CR2_STOP; // 1 stop bit
break;
}
// 1 stop bit: CR2 STOP[1:0] = 00 (default, so we can skip)
// Enable transmitter and receiver
USART1->CR1 |= USART_CR1_TE | USART_CR1_RE;
// Enable USART
USART1->CR1 |= USART_CR1_UE;
}
This is the function used to transfet the data throgh DMA
void MB_Frame_Transmit(volatile uint8_t *data, uint16_t len)
{
uart_tx_busy = 1;
SET_DE; // Enable RS485 Transmit mode
// Disable DMA channel before reconfiguring
DMA1_Channel2->CCR &= ~DMA_CCR_EN;
// Clear DMA interrupt flags for Channel 2
DMA1->IFCR = DMA_IFCR_CTCIF2 | DMA_IFCR_CTEIF2;
// Configure DMA Channel 2 for USART1_TX
DMA1_Channel2->CNDTR = len;
DMA1_Channel2->CPAR = (uint32_t)&USART1->TDR;
DMA1_Channel2->CMAR = (uint32_t)data;
// Reconfigure DMA Channel 2
DMA1_Channel2->CCR =
DMA_CCR_MINC | // Memory increment
DMA_CCR_DIR | // Read from memory (TX)
/*DMA_CCR_TCIE | // Enable transfer complete interrupt*/
DMA_CCR_PL_1; // High priority (optional)
// Enable USART1 TX DMA mode
USART1->CR3 |= USART_CR3_DMAT;
// Enable DMA Channel 2
DMA1_Channel2->CCR |= DMA_CCR_EN;
}
This is the ISR
void DMA1_Channel2_3_IRQHandler(void)
{
// Check Transfer Complete interrupt for Channel 2
if (DMA1->ISR & DMA_ISR_TCIF2)
{
// Clear transfer complete flag
DMA1->IFCR = DMA_IFCR_CTCIF2;
// Disable DMA Channel 2 and USART DMA mode
DMA1_Channel2->CCR &= ~DMA_CCR_EN;
USART1->CR3 &= ~USART_CR3_DMAT;
uart_tx_busy = 0;
CLEAR_DE; // Set RS485 to Receive mode
}
// Optional: handle transfer error (TEIF2)
if (DMA1->ISR & DMA_ISR_TEIF2)
{
DMA1->IFCR = DMA_IFCR_CTEIF2;
// You can set an error flag or retry here
Switch_Reset_LED_ON;
}
}
I call the DMA1_Channel2_3_IRQHandler() function from main once in 600 mS. With this loop delay. I will not re initiate the DMA transfer before previous transfer is completed. delay_ms() is the blocking function implemented by timer 14.
Now the interesting part: If I disable the TCIE bit inise the MB_Frame_Transmit() function, DMA transfer happens perfectly once in 600ms. I probe this in my oscilloscope and confirm.
But if I enable TCIE, transmission happens only for first time when micro controller is restarted. Then it hangs.
Few more observations. This is my main function
int main(void)
{
Config_System_Clock();
Init_GPIOs();
Init_DMA();
Init_UART1();
Init_Tim14_1ms();
__enable_irq();
for (uint8_t i = 0; i < 10; ++i) { TX_Array[i] = i; }
//UART1_Transmit_DMA(TX_Array, 10);
SET_DE;
//Switch_Reset_LED_ON;
while(1)
{
MB_Frame_Transmit(TX_Array, 10);
Switch_Status_LED_ON; delay_ms(300);
Switch_Status_LED_OFF; delay_ms(300);
}
}When the TCIE is enabled, the status LED is turned ON then not turned OFF. When means just for one time Switch_Statsu_LED_ON funtion is executed once then nothing further. Also the Reset LED placed insde Error handler is not turned, ON. which means means that part of ISR is also not executed.
Please let me know, what is the issue in my code.
Thank you, Anesh S.
Solved! Go to Solution.
2025-05-20 1:56 AM - edited 2025-05-20 1:57 AM
> But why ISR is called immediately at time <= (length-2) of transmission?
That's when DMA finished its job.
The UART transmitter is initially empty and requests data from DMA through UART_SR.TXE, which indicates "UART TX holding register empty". DMA transfers that data into UART's holding register. UART transfers that byte rapidly from holding register into its shift register and starts to shift the bits out (i.e. transmit - note that UART baudrate is several orders of magnitude slower than the mcu system clock, so transmitting one single *bit* takes much much longer than transferring a whole byte by DMA). That means, that the UART holding register is empty again, UART_SR.TXE goes up, which triggers another byte to be transferred by DMA to the holding register, where it waits until the first byte gets completely shifted out from the shift register. It means, that DMA already transferred 2 bytes and UART barely started to transmit the first byte's startbit.
For longer arrays, this goes on, DMA is virtually always ahead of UART by 2 bytes, so it finishes its transfer 2 bytes before UART transmits the last byte's stopbit.
JW
2025-05-18 7:27 AM
Probably not hanging, but stuck in an IRQ storm. If sources of interrupts are not cleared it will keep re-entering the IRQ Handler and no foreground code execution will occur.
Check pending interrupts.
Toggle GPIO at every IRQ Handler entry, scope pin as it will be happening very fast.
Perhaps have a count, and stop and inspect in the debugger. Determine WHERE it is stuck.
Check perhaps also HT (Half Transfer)
2025-05-18 9:24 AM
Hello, I modified the ISR code to turn ON an LED and toggle another port pin. But none of these lines are executed. Before that I enabled TCIE.
I tried to debug code by STM32CubeIDE. Debug is not proceeding above the function MB_Frame_Transmit(TX_Array, 10);. Anyhow I am not fluent in debugging process.
Please let me know what is the next step to debug.
void DMA1_Channel2_3_IRQHandler(void)
{
Switch_Reset_LED_ON;
Toggle_Status_LED;
// Check Transfer Complete interrupt for Channel 2
if (DMA1->ISR & DMA_ISR_TCIF2)
{
// Clear transfer complete flag
DMA1->IFCR = DMA_IFCR_CTCIF2;
// Disable DMA Channel 2 and USART DMA mode
DMA1_Channel2->CCR &= ~DMA_CCR_EN;
USART1->CR3 &= ~USART_CR3_DMAT;
uart_tx_busy = 0;
CLEAR_DE; // Set RS485 to Receive mode
}
// Optional: handle transfer error (TEIF2)
if (DMA1->ISR & DMA_ISR_TEIF2)
{
DMA1->IFCR = DMA_IFCR_CTEIF2;
// You can set an error flag or retry here
}
}
2025-05-18 10:23 AM
Like I said, STOP the code in the DEBUGGER, and determine WHERE it is stuck.
Instrument things like Error_Handler() and HardFault_Handler(), or any place you have silent while(1) loops where it can stuck and die.
Add other instrumentation so you know what's going on without the debugger, these things are happening faster than you can react, so provide continuous output rather than dead-stop with break-points and single-stepping.
DMA will only reload / retrigger in CIRCULAR mode.
2025-05-18 12:24 PM
I surfed internet and I could add few functions of error handlers. Please pardon me if they are useless.
__attribute__((naked)) void HardFault_Handler(void)
{
__asm volatile
(
"movs r0, #4 \n"
"mov r1, lr \n"
"tst r0, r1 \n"
"beq _msp_used \n"
"mrs r0, psp \n"
"b HardFault_Handler_C \n"
"_msp_used: \n"
"mrs r0, msp \n"
"b HardFault_Handler_C \n"
);
}
void HardFault_Handler_C(uint32_t *stacked_regs)
{
// Extract stacked CPU registers at fault time
volatile uint32_t r0 = stacked_regs[0];
volatile uint32_t r1 = stacked_regs[1];
volatile uint32_t r2 = stacked_regs[2];
volatile uint32_t r3 = stacked_regs[3];
volatile uint32_t r12 = stacked_regs[4];
volatile uint32_t lr = stacked_regs[5]; // Link Register
volatile uint32_t pc = stacked_regs[6]; // Program Counter
volatile uint32_t psr = stacked_regs[7]; // Program Status Register
// Optional: Place breakpoint here to examine values in debugger
// You can also send them over UART or log to flash
(void)r0;
(void)r1;
(void)r2;
(void)r3;
(void)r12;
(void)lr;
(void)pc;
(void)psr;
// Stay here or call reset
Error_Handler();
}
void Error_Handler(void)
{
// Blink PB4 forever to indicate error
while (1)
{
Toggle_Reset_LED;
for (volatile uint32_t i = 0; i < 100000; i++); // Delay loop
}
}I thought atleast Reset LED will be toglling after the microcontroller is trapped by some error. But that did not happen.
Then I tried debugging with step in function. I tried to step into loine by line of MB_Frame_Transmit(). But at end of that function, even debug action is not able to step anyother location. all the options except cloing debug session will be greyed. I made a screen recording, uploaded in Youtube and shared the link below:
Further, I did not enable the DMA_CCR_TCIE bit and debugged. Now some issue happens inside my delay function. I uploaded this video too. The link is below:
Please pardon me if I dont understand even basics.
2025-05-19 1:34 PM
I think I have find the issue.
In startup_stm32f030c8tx.s I searched for ISR name "DMA1_Channel2_3_IRQHandler". That is not found. I used this wrong function name from ChatGPT :)
I could find similar function name as DMA1_CH2_3_IRQHandler. I used that. now ISR is called.
But now I have another issue. I make DE pin low inside ISR. I expect DE pin toi be logic low adter all the 10 elements are transmitted. But after 8 elements are transmitted the DE pin is made low.
Then I placed a blocking while function inside ISR as below:
void DMA1_CH2_3_IRQHandler(void)
{
//Switch_Reset_LED_ON;
//Toggle_Status_LED;
// Check Transfer Complete interrupt for Channel 2
if (DMA1->ISR & DMA_ISR_TCIF2)
{
// Clear transfer complete flag
DMA1->IFCR = DMA_IFCR_CTCIF2;
// Disable DMA Channel 2 and USART DMA mode
DMA1_Channel2->CCR &= ~DMA_CCR_EN;
USART1->CR3 &= ~USART_CR3_DMAT;
while (!(USART1->ISR & USART_ISR_TC));
uart_tx_busy = 0;
CLEAR_DE; // Set RS485 to Receive mode
}
// Optional: handle transfer error (TEIF2)
if (DMA1->ISR & DMA_ISR_TEIF2)
{
DMA1->IFCR = DMA_IFCR_CTEIF2;
// You can set an error flag or retry here
}
}
The DE is made logic 0 after all the frames are completed. I am not able to understand this behaviuour. PLease refer the plot wothout while loop.
When I debugged step by step, DE pin is handled correctly. why?
I dont want the blocking while function inside the interrupt. Infact I dont want blocking fuctions anywhere.
Please let me know whats going on wrong here.
Thank you, Anesh S.
2025-05-19 10:21 PM
For your reference I have provided my complete code.
My micro controller is STM32F030C8T6
#include <stdint.h>
#include <stddef.h>
#include "stm32f030x8.h"
#define Set_USART1_BRR (40000000/9600) // 9600 Baudrate
#define Set_Parity 0x01 // EVen
#define DMA1_Channel2_ISR_TCIF DMA_ISR_TCIF2 // Transfer complete flag for channel 2
#define DMA1_Channel2_IFCR_CTCIF DMA_IFCR_CTCIF2 // Clear transfer complete flag channel 2
#define Switch_Reset_LED_ON (GPIOB->BSRR = GPIO_BSRR_BS_10) // PB10 (Set pin)
#define Switch_Status_LED_ON (GPIOB->BSRR = GPIO_BSRR_BS_4) // PB4 (Set pin)
#define Switch_RXD_LED_ON (GPIOB->BSRR = GPIO_BSRR_BS_3) // PB3 (Set pin)
#define Switch_TXD_LED_ON (GPIOA->BSRR = GPIO_BSRR_BS_15) // PA15 (Set pin)
#define Switch_Reset_LED_OFF (GPIOB->BSRR = GPIO_BSRR_BR_10) // PB10 (Set pin)
#define Switch_Status_LED_OFF (GPIOB->BSRR = GPIO_BSRR_BR_4) // PB4 (Set pin)
#define Switch_RXD_LED_OFF (GPIOB->BSRR = GPIO_BSRR_BR_3) // PB3 (Set pin)
#define Switch_TXD_LED_OFF (GPIOA->BSRR = GPIO_BSRR_BR_15) // PA15 (Set pin)
#define Toggle_Reset_LED (GPIOB->ODR ^= GPIO_ODR_10) // PB10 (Set pin)
#define Toggle_Status_LED (GPIOB->ODR ^= GPIO_ODR_4)
#define CLEAR_DE (GPIOB->ODR &= ~(1 << 5));
#define SET_DE (GPIOB->ODR |= (1 << 5));
void Config_System_Clock(void);
void Init_GPIOs(void);
void Init_DMA(void);
void Init_UART1(void);
void MB_Frame_Transmit(volatile uint8_t *pData, uint16_t size);
void Init_Tim14_1ms(void);
void delay_ms(uint32_t ms);
void Error_Handler(void);
void block_delay_500ms_for_loop(void);
volatile uint32_t ms_Ticks;
volatile uint8_t Tick_1ms;
volatile uint8_t TX_Array[10]={0}, RX_Array[10]={0};
volatile uint8_t uart_tx_busy = 0;
int main(void)
{
Config_System_Clock();
Init_GPIOs();
Init_DMA();
Init_UART1();
//Init_Tim14_1ms();
__enable_irq();
for (uint8_t i = 0; i < 10; ++i) { TX_Array[i] = i; }
//UART1_Transmit_DMA(TX_Array, 10);
//Switch_Reset_LED_ON;
while(1)
{
MB_Frame_Transmit(TX_Array, 1); block_delay_500ms_for_loop();
//Switch_Status_LED_ON; delay_ms(300);
//Switch_Status_LED_OFF; delay_ms(300);
//Toggle_Reset_LED;
}
}
void Init_GPIOs(void)
{
RCC->AHBENR |= RCC_AHBENR_GPIOAEN; // Enable GPIOA clock
RCC->AHBENR |= RCC_AHBENR_GPIOBEN; // Enable GPIOB clock
RCC->AHBENR |= RCC_AHBENR_GPIOCEN; // Enable GPIOC clock
/* Settings for ONB_Reset_LED: PB10 */
GPIOB->MODER &= ~GPIO_MODER_MODER10; // Clear mode for PB10
GPIOB->MODER |= GPIO_MODER_MODER10_0; // Set as Output (01)
GPIOB->OTYPER &= ~GPIO_OTYPER_OT_10; // Push-pull (0)
GPIOB->OSPEEDR &= ~GPIO_OSPEEDR_OSPEEDR10; // Clear speed for PB10
GPIOB->OSPEEDR |= GPIO_OSPEEDR_OSPEEDR10_0; // Medium speed (01)
GPIOB->PUPDR &= ~GPIO_PUPDR_PUPDR10; // No pull-up, no pull-down (00)
/* Settings for ONB_Status_LED: PB4 */
GPIOB->MODER &= ~GPIO_MODER_MODER4; // Clear mode for PB4
GPIOB->MODER |= GPIO_MODER_MODER4_0; // Set as Output (01)
GPIOB->OTYPER &= ~GPIO_OTYPER_OT_4; // Push-pull (0)
GPIOB->OSPEEDR &= ~GPIO_OSPEEDR_OSPEEDR4; // Clear speed for PB4
GPIOB->OSPEEDR |= GPIO_OSPEEDR_OSPEEDR4_0; // Medium speed (01)
GPIOB->PUPDR &= ~GPIO_PUPDR_PUPDR4; // No pull-up, no pull-down (00)
/* Settings for ONB_RXD_LED: PB3 */
GPIOB->MODER &= ~GPIO_MODER_MODER3; // Clear mode for PB3
GPIOB->MODER |= GPIO_MODER_MODER3_0; // Set as Output (01)
GPIOB->OTYPER &= ~GPIO_OTYPER_OT_3; // Push-pull (0)
GPIOB->OSPEEDR &= ~GPIO_OSPEEDR_OSPEEDR3; // Clear speed for PB3
GPIOB->OSPEEDR |= GPIO_OSPEEDR_OSPEEDR3_0; // Medium speed (01)
GPIOB->PUPDR &= ~GPIO_PUPDR_PUPDR3; // No pull-up, no pull-down (00)
/* Settings for ONB_TXD_LED: PA15 */
GPIOA->MODER &= ~GPIO_MODER_MODER15; // Clear mode for PA15
GPIOA->MODER |= GPIO_MODER_MODER15_0; // Set as Output (01)
GPIOA->OTYPER &= ~GPIO_OTYPER_OT_15; // Push-pull (0)
GPIOA->OSPEEDR &= ~GPIO_OSPEEDR_OSPEEDR15; // Clear speed for PA15
GPIOA->OSPEEDR |= GPIO_OSPEEDR_OSPEEDR15_0; // Medium speed (01)
GPIOA->PUPDR &= ~GPIO_PUPDR_PUPDR15; // No pull-up, no pull-down (00)
}
void Init_DMA(void)
{
// Enable clock for DMA1 peripheral by setting the DMA1EN bit in RCC AHBENR register
RCC->AHBENR |= RCC_AHBENR_DMA1EN;
NVIC_ClearPendingIRQ(DMA1_Channel2_3_IRQn);
NVIC_SetPriority(DMA1_Channel2_3_IRQn, 0);
NVIC_EnableIRQ(DMA1_Channel2_3_IRQn);
}
void Init_UART1(void)
{
// 1. Enable clocks for GPIOB, USART1, and DMA1
RCC->AHBENR |= RCC_AHBENR_GPIOBEN;
RCC->APB2ENR |= RCC_APB2ENR_USART1EN;
// 2. Configure PB5 as DE output (push-pull, high speed)
GPIOB->MODER &= ~(3 << (5 * 2));
GPIOB->MODER |= (1 << (5 * 2)); // Output mode
GPIOB->OTYPER &= ~(1 << 5); // Push-pull
GPIOB->OSPEEDR |= (3 << (5 * 2)); // High speed
GPIOB->PUPDR &= ~(3 << (5 * 2)); // No pull
GPIOB->ODR &= ~(1 << 5); // Set DE LOW (receive mode)
// 3. Configure PB6 as USART1_TX (AF0)
GPIOB->MODER &= ~(3 << (6 * 2));
GPIOB->MODER |= (2 << (6 * 2)); // Alternate function
GPIOB->OTYPER &= ~(1 << 6); // Push-pull
GPIOB->OSPEEDR |= (3 << (6 * 2)); // High speed
GPIOB->PUPDR &= ~(3 << (6 * 2));
GPIOB->PUPDR |= (1 << (6 * 2)); // Pull-up
GPIOB->AFR[0] &= ~(0xF << (6 * 4));
GPIOB->AFR[0] |= (0x0 << (6 * 4)); // AF0 = USART1
// Reset USART1
USART1->CR1 = 0;
USART1->CR2 = 0;
USART1->CR3 = 0;
USART1->BRR = Set_USART1_BRR; // Set baud rate
switch (Set_Parity)
{
case 0: // 8N2 (No parity, 2 stop bits)
USART1->CR1 &= ~USART_CR1_PCE;
USART1->CR1 &= ~USART_CR1_M;
USART1->CR2 &= ~USART_CR2_STOP;
USART1->CR2 |= USART_CR2_STOP_1 | USART_CR2_STOP_0; // 2 stop bits
break;
case 1: // 8E1 (Even parity, 1 stop bit)
USART1->CR1 |= USART_CR1_PCE;
USART1->CR1 &= ~USART_CR1_PS;
USART1->CR1 |= USART_CR1_M;
USART1->CR2 &= ~USART_CR2_STOP; // 1 stop bit
break;
case 2: // 8O1 (Odd parity, 1 stop bit)
USART1->CR1 |= USART_CR1_PCE;
USART1->CR1 |= USART_CR1_PS;
USART1->CR1 |= USART_CR1_M;
USART1->CR2 &= ~USART_CR2_STOP; // 1 stop bit
break;
}
// 1 stop bit: CR2 STOP[1:0] = 00 (default, so we can skip)
// Enable transmitter and receiver
USART1->CR1 |= USART_CR1_TE | USART_CR1_RE;
// Enable USART
USART1->CR1 |= USART_CR1_UE;
}
void MB_Frame_Transmit(volatile uint8_t *data, uint16_t len)
{
uart_tx_busy = 1;
SET_DE; // Enable RS485 Transmit mode
// Disable DMA channel before reconfiguring
DMA1_Channel2->CCR &= ~DMA_CCR_EN;
// Clear DMA interrupt flags for Channel 2
DMA1->IFCR = DMA_IFCR_CTCIF2 | DMA_IFCR_CTEIF2;
// Configure DMA Channel 2 for USART1_TX
DMA1_Channel2->CNDTR = len;
DMA1_Channel2->CPAR = (uint32_t)&USART1->TDR;
DMA1_Channel2->CMAR = (uint32_t)data;
// Reconfigure DMA Channel 2
DMA1_Channel2->CCR =
DMA_CCR_MINC | // Memory increment
DMA_CCR_DIR | // Read from memory (TX)
DMA_CCR_TCIE | // Enable transfer complete interrupt
DMA_CCR_PL_1; // High priority (optional)
// Enable USART1 TX DMA mode
USART1->CR3 |= USART_CR3_DMAT;
// Enable DMA Channel 2
DMA1_Channel2->CCR |= DMA_CCR_EN;
}
void DMA1_CH2_3_IRQHandler(void)
{
//Switch_Reset_LED_ON;
//Toggle_Status_LED;
// Check Transfer Complete interrupt for Channel 2
if (DMA1->ISR & DMA_ISR_TCIF2)
{
// Clear transfer complete flag
DMA1->IFCR = DMA_IFCR_CTCIF2;
// Disable DMA Channel 2 and USART DMA mode
DMA1_Channel2->CCR &= ~DMA_CCR_EN;
USART1->CR3 &= ~USART_CR3_DMAT;
//while (!(USART1->ISR & USART_ISR_TC));
uart_tx_busy = 0;
CLEAR_DE; // Set RS485 to Receive mode
}
// Optional: handle transfer error (TEIF2)
if (DMA1->ISR & DMA_ISR_TEIF2)
{
DMA1->IFCR = DMA_IFCR_CTEIF2;
// You can set an error flag or retry here
}
}
__attribute__((naked)) void HardFault_Handler(void)
{
__asm volatile
(
"movs r0, #4 \n"
"mov r1, lr \n"
"tst r0, r1 \n"
"beq _msp_used \n"
"mrs r0, psp \n"
"b HardFault_Handler_C \n"
"_msp_used: \n"
"mrs r0, msp \n"
"b HardFault_Handler_C \n"
);
}
void HardFault_Handler_C(uint32_t *stacked_regs)
{
// Extract stacked CPU registers at fault time
volatile uint32_t r0 = stacked_regs[0];
volatile uint32_t r1 = stacked_regs[1];
volatile uint32_t r2 = stacked_regs[2];
volatile uint32_t r3 = stacked_regs[3];
volatile uint32_t r12 = stacked_regs[4];
volatile uint32_t lr = stacked_regs[5]; // Link Register
volatile uint32_t pc = stacked_regs[6]; // Program Counter
volatile uint32_t psr = stacked_regs[7]; // Program Status Register
// Optional: Place breakpoint here to examine values in debugger
// You can also send them over UART or log to flash
(void)r0;
(void)r1;
(void)r2;
(void)r3;
(void)r12;
(void)lr;
(void)pc;
(void)psr;
// Stay here or call reset
Error_Handler();
}
void Error_Handler(void)
{
// Blink PB4 forever to indicate error
while (1)
{
Toggle_Reset_LED;
for (volatile uint32_t i = 0; i < 100000; i++); // Delay loop
}
}
void Init_Tim14_1ms(void)
{
RCC->APB1ENR |= RCC_APB1ENR_TIM14EN;
TIM14->PSC = 39;
TIM14->ARR = 999;
TIM14->CNT = 0;
TIM14->SR &= ~TIM_SR_UIF; // Clear any pending flag
TIM14->DIER |= TIM_DIER_UIE; // Update interrupt enable
TIM14->CR1 |= TIM_CR1_CEN; // Counter enable
NVIC_EnableIRQ(TIM14_IRQn); // Enable IRQ in NVIC
}
void TIM14_IRQHandler(void)
{
if (TIM14->SR & TIM_SR_UIF)
{
//Switch_Status_LED_ON;
TIM14->SR &= ~TIM_SR_UIF;
ms_Ticks++;
Tick_1ms=1;
//Switch_Status_LED_OFF;
}
}
void delay_ms(uint32_t ms)
{
uint32_t start = ms_Ticks;
while ((ms_Ticks - start) < ms);
}
void Config_System_Clock(void)
{
// 1. Enable HSE (High Speed External oscillator)
RCC->CR |= RCC_CR_HSEON;
while ((RCC->CR & RCC_CR_HSERDY) == 0); // Wait for HSE ready
// 2. Configure PLL
// PLL source = HSE, PLL multiplier = 5
RCC->CFGR &= ~(RCC_CFGR_PLLSRC | RCC_CFGR_PLLMUL); // Clear PLL config
RCC->CFGR |= RCC_CFGR_PLLSRC_HSE_PREDIV | RCC_CFGR_PLLMUL5; // HSE / 1 * 5
// 3. Enable PLL
RCC->CR |= RCC_CR_PLLON;
while ((RCC->CR & RCC_CR_PLLRDY) == 0); // Wait for PLL ready
// 4. Select PLL as system clock
RCC->CFGR &= ~RCC_CFGR_SW;
RCC->CFGR |= RCC_CFGR_SW_PLL;
while ((RCC->CFGR & RCC_CFGR_SWS) != RCC_CFGR_SWS_PLL); // Wait until PLL used as system clock
}
void block_delay_500ms_for_loop(void)
{
for (uint32_t i = 0; i < 5000001; i++)
{
__NOP();
}
}When I reduced of array to 5, CLEAR_DE is executed at end of third element.
When I reduced the length to 2, the CLEAR_DE is switched off at 4 micro seconds (almost immediate). This time may be time to initiate the DMA and immediate execution of ISR. Same behaviour happens when I reduced the length to 1. So This behavior i solid.
But why ISR is called immediately at time <= (length-2) of transmission?
Please let me know what is going on wrong.
2025-05-20 1:56 AM - edited 2025-05-20 1:57 AM
> But why ISR is called immediately at time <= (length-2) of transmission?
That's when DMA finished its job.
The UART transmitter is initially empty and requests data from DMA through UART_SR.TXE, which indicates "UART TX holding register empty". DMA transfers that data into UART's holding register. UART transfers that byte rapidly from holding register into its shift register and starts to shift the bits out (i.e. transmit - note that UART baudrate is several orders of magnitude slower than the mcu system clock, so transmitting one single *bit* takes much much longer than transferring a whole byte by DMA). That means, that the UART holding register is empty again, UART_SR.TXE goes up, which triggers another byte to be transferred by DMA to the holding register, where it waits until the first byte gets completely shifted out from the shift register. It means, that DMA already transferred 2 bytes and UART barely started to transmit the first byte's startbit.
For longer arrays, this goes on, DMA is virtually always ahead of UART by 2 bytes, so it finishes its transfer 2 bytes before UART transmits the last byte's stopbit.
JW
2025-05-20 10:55 AM - edited 2025-05-20 11:03 AM
Thank you for detailed information. Now I have implemented using USART_ISR_TC of UART1. I probed all the functions by place port pin on/off commands. Both the ISRs are working fine. I think I can handle even without ISR by DMA.
Anyhow, I left it to be in code, Inside this ISR I enabled USART_ISR_TC. I hope nothing will be hurt.
I post my complete code here of TX with DMA. I request you to have a look for any potential issues.
#include <stdint.h>
#include <stddef.h>
#include "stm32f030x8.h"
#define Set_USART1_BRR (40000000/9600) // 9600 Baudrate
#define Set_Parity 0x01 // EVen
#define DMA1_Channel2_ISR_TCIF DMA_ISR_TCIF2 // Transfer complete flag for channel 2
#define DMA1_Channel2_IFCR_CTCIF DMA_IFCR_CTCIF2 // Clear transfer complete flag channel 2
#define Switch_Reset_LED_ON (GPIOB->BSRR = GPIO_BSRR_BS_10) // PB10 (Set pin)
#define Switch_Status_LED_ON (GPIOB->BSRR = GPIO_BSRR_BS_4) // PB4 (Set pin)
#define Switch_RXD_LED_ON (GPIOB->BSRR = GPIO_BSRR_BS_3) // PB3 (Set pin)
#define Switch_TXD_LED_ON (GPIOA->BSRR = GPIO_BSRR_BS_15) // PA15 (Set pin)
#define Switch_Reset_LED_OFF (GPIOB->BSRR = GPIO_BSRR_BR_10) // PB10 (Set pin)
#define Switch_Status_LED_OFF (GPIOB->BSRR = GPIO_BSRR_BR_4) // PB4 (Set pin)
#define Switch_RXD_LED_OFF (GPIOB->BSRR = GPIO_BSRR_BR_3) // PB3 (Set pin)
#define Switch_TXD_LED_OFF (GPIOA->BSRR = GPIO_BSRR_BR_15) // PA15 (Set pin)
#define Toggle_Reset_LED (GPIOB->ODR ^= GPIO_ODR_10) // PB10 (Set pin)
#define Toggle_Status_LED (GPIOB->ODR ^= GPIO_ODR_4)
#define CLEAR_DE (GPIOB->ODR &= ~(1 << 5));
#define SET_DE (GPIOB->ODR |= (1 << 5));
void Config_System_Clock(void);
void Init_GPIOs(void);
void Init_DMA(void);
void Init_UART1(void);
void MB_Frame_Transmit(volatile uint8_t *pData, uint16_t size);
void Init_Tim14_1ms(void);
void delay_ms(uint32_t ms);
void Error_Handler(void);
void block_delay_500ms_for_loop(void);
volatile uint32_t Ticks_1ms, Ticks_100ms;
volatile uint8_t Flag_1ms, Flag_100ms;
volatile uint8_t TX_Array[10]={0}, RX_Array[10]={0};
volatile uint8_t uart_tx_busy = 0;
int main(void)
{
Config_System_Clock();
Init_GPIOs();
Init_DMA();
Init_UART1();
Init_Tim14_1ms();
__enable_irq();
for (uint8_t i = 0; i < 10; ++i) { TX_Array[i] = i; }
//UART1_Transmit_DMA(TX_Array, 10);
//Switch_Reset_LED_ON;
while(1)
{
if(Flag_100ms)
{
MB_Frame_Transmit(TX_Array, 10);
Flag_100ms=0;
}
//block_delay_500ms_for_loop();
//Switch_Status_LED_ON; delay_ms(300);
//Switch_Status_LED_OFF; delay_ms(300);
//Toggle_Reset_LED;
if(Flag_1ms)
{
Toggle_Status_LED;
Flag_1ms=0;
}
}
}
void Init_GPIOs(void)
{
RCC->AHBENR |= RCC_AHBENR_GPIOAEN; // Enable GPIOA clock
RCC->AHBENR |= RCC_AHBENR_GPIOBEN; // Enable GPIOB clock
RCC->AHBENR |= RCC_AHBENR_GPIOCEN; // Enable GPIOC clock
/* Settings for ONB_Reset_LED: PB10 */
GPIOB->MODER &= ~GPIO_MODER_MODER10; // Clear mode for PB10
GPIOB->MODER |= GPIO_MODER_MODER10_0; // Set as Output (01)
GPIOB->OTYPER &= ~GPIO_OTYPER_OT_10; // Push-pull (0)
GPIOB->OSPEEDR &= ~GPIO_OSPEEDR_OSPEEDR10; // Clear speed for PB10
GPIOB->OSPEEDR |= GPIO_OSPEEDR_OSPEEDR10_0; // Medium speed (01)
GPIOB->PUPDR &= ~GPIO_PUPDR_PUPDR10; // No pull-up, no pull-down (00)
/* Settings for ONB_Status_LED: PB4 */
GPIOB->MODER &= ~GPIO_MODER_MODER4; // Clear mode for PB4
GPIOB->MODER |= GPIO_MODER_MODER4_0; // Set as Output (01)
GPIOB->OTYPER &= ~GPIO_OTYPER_OT_4; // Push-pull (0)
GPIOB->OSPEEDR &= ~GPIO_OSPEEDR_OSPEEDR4; // Clear speed for PB4
GPIOB->OSPEEDR |= GPIO_OSPEEDR_OSPEEDR4_0; // Medium speed (01)
GPIOB->PUPDR &= ~GPIO_PUPDR_PUPDR4; // No pull-up, no pull-down (00)
/* Settings for ONB_RXD_LED: PB3 */
GPIOB->MODER &= ~GPIO_MODER_MODER3; // Clear mode for PB3
GPIOB->MODER |= GPIO_MODER_MODER3_0; // Set as Output (01)
GPIOB->OTYPER &= ~GPIO_OTYPER_OT_3; // Push-pull (0)
GPIOB->OSPEEDR &= ~GPIO_OSPEEDR_OSPEEDR3; // Clear speed for PB3
GPIOB->OSPEEDR |= GPIO_OSPEEDR_OSPEEDR3_0; // Medium speed (01)
GPIOB->PUPDR &= ~GPIO_PUPDR_PUPDR3; // No pull-up, no pull-down (00)
/* Settings for ONB_TXD_LED: PA15 */
GPIOA->MODER &= ~GPIO_MODER_MODER15; // Clear mode for PA15
GPIOA->MODER |= GPIO_MODER_MODER15_0; // Set as Output (01)
GPIOA->OTYPER &= ~GPIO_OTYPER_OT_15; // Push-pull (0)
GPIOA->OSPEEDR &= ~GPIO_OSPEEDR_OSPEEDR15; // Clear speed for PA15
GPIOA->OSPEEDR |= GPIO_OSPEEDR_OSPEEDR15_0; // Medium speed (01)
GPIOA->PUPDR &= ~GPIO_PUPDR_PUPDR15; // No pull-up, no pull-down (00)
}
void Init_DMA(void)
{
// Enable clock for DMA1
RCC->AHBENR |= RCC_AHBENR_DMA1EN;
// Optional: Preconfigure TX DMA Channel2 default settings (actual values set during transmit)
DMA1_Channel2->CCR = 0; // Disable first
DMA1_Channel2->CNDTR = 0;
DMA1_Channel2->CPAR = (uint32_t)&USART1->TDR;
DMA1_Channel2->CMAR = 0;
DMA1_Channel2->CCR =
DMA_CCR_MINC | // Memory increment mode
DMA_CCR_DIR | // Read from memory (TX)
DMA_CCR_TCIE | // Transfer complete interrupt
DMA_CCR_PL_1; // High priority
// Clear any pending DMA interrupt flags
DMA1->IFCR = DMA_IFCR_CTCIF2 | DMA_IFCR_CTEIF2;
// Configure NVIC for DMA Channel 2/3 interrupt
NVIC_ClearPendingIRQ(DMA1_Channel2_3_IRQn);
NVIC_SetPriority(DMA1_Channel2_3_IRQn, 0);
NVIC_EnableIRQ(DMA1_Channel2_3_IRQn);
}
void Init_UART1(void)
{
// 1. Enable clocks
RCC->AHBENR |= RCC_AHBENR_GPIOBEN;
RCC->APB2ENR |= RCC_APB2ENR_USART1EN;
// 2. Configure PB5 as DE (output, push-pull, high speed)
GPIOB->MODER &= ~(3 << (5 * 2));
GPIOB->MODER |= (1 << (5 * 2));
GPIOB->OTYPER &= ~(1 << 5);
GPIOB->OSPEEDR |= (3 << (5 * 2));
GPIOB->PUPDR &= ~(3 << (5 * 2));
GPIOB->ODR &= ~(1 << 5); // Set DE low initially
// 3. Configure PB6 as USART1_TX (AF0)
GPIOB->MODER &= ~(3 << (6 * 2));
GPIOB->MODER |= (2 << (6 * 2)); // Alternate function
GPIOB->OTYPER &= ~(1 << 6);
GPIOB->OSPEEDR |= (3 << (6 * 2));
GPIOB->PUPDR &= ~(3 << (6 * 2));
GPIOB->PUPDR |= (1 << (6 * 2)); // Pull-up
GPIOB->AFR[0] &= ~(0xF << (6 * 4));
GPIOB->AFR[0] |= (0x0 << (6 * 4)); // AF0
// 4. Reset USART1 registers safely (only if USART is disabled)
if (!(USART1->CR1 & USART_CR1_UE))
{
USART1->CR1 = 0;
USART1->CR2 = 0;
USART1->CR3 = 0;
}
// 5. Clear status flags
volatile uint32_t tmp;
tmp = USART1->ISR;
tmp = USART1->RDR;
(void)tmp;
// 6. Set baud rate
USART1->BRR = Set_USART1_BRR;
// 7. Configure parity and stop bits
switch (Set_Parity)
{
case 0: // 8N2
USART1->CR1 &= ~USART_CR1_PCE;
USART1->CR1 &= ~USART_CR1_M;
USART1->CR2 &= ~USART_CR2_STOP;
USART1->CR2 |= USART_CR2_STOP_1 | USART_CR2_STOP_0;
break;
case 1: // 8E1
USART1->CR1 |= USART_CR1_PCE;
USART1->CR1 &= ~USART_CR1_PS;
USART1->CR1 |= USART_CR1_M;
USART1->CR2 &= ~USART_CR2_STOP;
break;
case 2: // 8O1
USART1->CR1 |= USART_CR1_PCE;
USART1->CR1 |= USART_CR1_PS;
USART1->CR1 |= USART_CR1_M;
USART1->CR2 &= ~USART_CR2_STOP;
break;
}
// 8. Enable TX and RX
USART1->CR1 |= USART_CR1_TE | USART_CR1_RE;
// 9. Enable USART1 interrupt (for TCIE used in TX complete)
NVIC_ClearPendingIRQ(USART1_IRQn);
NVIC_SetPriority(USART1_IRQn, 1);
NVIC_EnableIRQ(USART1_IRQn);
// 10. Enable USART1
USART1->CR1 |= USART_CR1_UE;
}
void MB_Frame_Transmit(volatile uint8_t *data, uint16_t len)
{
//Switch_Status_LED_ON;
uart_tx_busy = 1;
SET_DE; // Enable RS485 transmit mode
// Disable DMA channel before reconfiguration
DMA1_Channel2->CCR &= ~DMA_CCR_EN;
// Clear DMA Channel 2 interrupt flags
DMA1->IFCR = DMA_IFCR_CTCIF2 | DMA_IFCR_CTEIF2;
// Configure DMA for USART1_TX
DMA1_Channel2->CPAR = (uint32_t)&USART1->TDR;
DMA1_Channel2->CMAR = (uint32_t)data;
DMA1_Channel2->CNDTR = len;
DMA1_Channel2->CCR =
DMA_CCR_MINC | // Memory increment mode
DMA_CCR_DIR | // Read from memory
DMA_CCR_TCIE | // Enable transfer complete interrupt
DMA_CCR_PL_1; // High priority (optional)
// Enable USART1 DMA TX
USART1->CR3 |= USART_CR3_DMAT;
// Enable DMA channel
DMA1_Channel2->CCR |= DMA_CCR_EN;
//Switch_Status_LED_OFF;
}
void DMA1_CH2_3_IRQHandler(void)
{
uint32_t isr = DMA1->ISR;
if (isr & DMA_ISR_TCIF2)
{
//Switch_Status_LED_ON;
// Clear transfer complete flag and disable DMA
DMA1->IFCR = DMA_IFCR_CTCIF2;
DMA1_Channel2->CCR &= ~DMA_CCR_EN;
USART1->CR3 &= ~USART_CR3_DMAT;
// Enable USART TC interrupt to detect final byte transmission on the line
USART1->CR1 |= USART_CR1_TCIE;
//Switch_Status_LED_OFF;
}
if (isr & DMA_ISR_TEIF2)
{
DMA1->IFCR = DMA_IFCR_CTEIF2;
// Optional: set error flag or retry logic
}
}
void USART1_IRQHandler(void)
{
uint32_t isr = USART1->ISR;
volatile uint32_t dummy;
// Handle Transmission Complete
if (isr & USART_ISR_TC)
{
//Switch_Status_LED_ON;
USART1->ICR = USART_ICR_TCCF; // Clear Transmission Complete
USART1->CR1 &= ~USART_CR1_TCIE; // Disable TC interrupt
CLEAR_DE; // Return RS485 to receive mode
uart_tx_busy = 0;
Toggle_Reset_LED;
//Switch_Status_LED_OFF;
}
// Just clear **all** USART error flags if any error is present
if (isr & (USART_ISR_PE | USART_ISR_FE | USART_ISR_NE | USART_ISR_ORE))
{
USART1->ICR = USART_ICR_PECF | USART_ICR_FECF | USART_ICR_NCF | USART_ICR_ORECF; // Clear all errors
dummy = USART1->RDR; // Read RDR to clear error conditions
(void)dummy;
}
}
__attribute__((naked)) void HardFault_Handler(void)
{
__asm volatile
(
"movs r0, #4 \n"
"mov r1, lr \n"
"tst r0, r1 \n"
"beq _msp_used \n"
"mrs r0, psp \n"
"b HardFault_Handler_C \n"
"_msp_used: \n"
"mrs r0, msp \n"
"b HardFault_Handler_C \n"
);
}
void HardFault_Handler_C(uint32_t *stacked_regs)
{
// Extract stacked CPU registers at fault time
volatile uint32_t r0 = stacked_regs[0];
volatile uint32_t r1 = stacked_regs[1];
volatile uint32_t r2 = stacked_regs[2];
volatile uint32_t r3 = stacked_regs[3];
volatile uint32_t r12 = stacked_regs[4];
volatile uint32_t lr = stacked_regs[5]; // Link Register
volatile uint32_t pc = stacked_regs[6]; // Program Counter
volatile uint32_t psr = stacked_regs[7]; // Program Status Register
// Optional: Place breakpoint here to examine values in debugger
// You can also send them over UART or log to flash
(void)r0;
(void)r1;
(void)r2;
(void)r3;
(void)r12;
(void)lr;
(void)pc;
(void)psr;
// Stay here or call reset
Error_Handler();
}
void Error_Handler(void)
{
// Blink PB4 forever to indicate error
while (1)
{
Toggle_Reset_LED;
for (volatile uint32_t i = 0; i < 100000; i++); // Delay loop
}
}
void Init_Tim14_1ms(void)
{
RCC->APB1ENR |= RCC_APB1ENR_TIM14EN;
TIM14->PSC = 39;
TIM14->ARR = 999;
TIM14->CNT = 0;
TIM14->SR &= ~TIM_SR_UIF; // Clear any pending flag
TIM14->DIER |= TIM_DIER_UIE; // Update interrupt enable
TIM14->CR1 |= TIM_CR1_CEN; // Counter enable
NVIC_EnableIRQ(TIM14_IRQn); // Enable IRQ in NVIC
}
void TIM14_IRQHandler(void)
{
if (TIM14->SR & TIM_SR_UIF)
{
TIM14->SR &= ~TIM_SR_UIF; // Clear update interrupt flag
Ticks_1ms++; // Optional global ms counter
Flag_1ms = 1; // Set 1ms flag
// Increment 100ms counter and set flag when 100ms elapsed
if (++Ticks_100ms >= 100)
{
Flag_100ms = 1;
Ticks_100ms = 0; // Reset for next 100 ms period
}
}
}
void delay_ms(uint32_t ms)
{
uint32_t start = Ticks_1ms;
while ((Ticks_1ms - start) < ms);
}
void Config_System_Clock(void)
{
// 1. Enable HSE (High Speed External oscillator)
RCC->CR |= RCC_CR_HSEON;
while ((RCC->CR & RCC_CR_HSERDY) == 0); // Wait for HSE ready
// 2. Configure PLL
// PLL source = HSE, PLL multiplier = 5
RCC->CFGR &= ~(RCC_CFGR_PLLSRC | RCC_CFGR_PLLMUL); // Clear PLL config
RCC->CFGR |= RCC_CFGR_PLLSRC_HSE_PREDIV | RCC_CFGR_PLLMUL5; // HSE / 1 * 5
// 3. Enable PLL
RCC->CR |= RCC_CR_PLLON;
while ((RCC->CR & RCC_CR_PLLRDY) == 0); // Wait for PLL ready
// 4. Select PLL as system clock
RCC->CFGR &= ~RCC_CFGR_SW;
RCC->CFGR |= RCC_CFGR_SW_PLL;
while ((RCC->CFGR & RCC_CFGR_SWS) != RCC_CFGR_SWS_PLL); // Wait until PLL used as system clock
}
void block_delay_500ms_for_loop(void)
{
for (uint32_t i = 0; i < 5000001; i++)
{
__NOP();
}
}Now I started implementing RX via DMA.
Thank you.
2025-05-20 11:10 AM
While Tx is fully under the mcu's control and so DMA is relatively straighforward; Rx through DMA is tricky, as it operates on data from outside, which may be corrupted. Some folks combine Rx DMA with timeouts (often in the form of the UART's IDLE feature), but I personally simply don't use DMA and handle it in interrupt. UART is relatively slow.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.