2024-01-10 10:46 AM
i have established communication with a BLDC (Brushless DC) controller. Initially, i send a message to the controller using the function void sendParameter(uint8_t parameter). Following this transmission, the BLDC controller is expected to respond with a frame. Although the transmission process appears to be functioning correctly, the receiver is not operating as expected. i have confirmed this issue using a logic analyzer.
UART_HandleTypeDef huart1;
uint8_t buffer[10];
uint8_t senddata[4] = {0x66, 0x42, 0x00, 0xA8};
uint8_t transmitAllowed = 1;
-----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART1_UART_Init(void)
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
HAL_UART_Receive_IT(&huart1, buffer, 1);
}
void sendParameter(uint8_t parameter)
{
HAL_UART_Transmit_IT(&huart1, senddata, 4);
HAL_Delay(100);
}
*/
int main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_USART1_UART_Init();
HAL_UART_Receive_IT(&huart1, buffer, 10);
while (1)
{
readParameter(0x42);
}
Solved! Go to Solution.
2024-01-11 12:13 AM
If it didn't enter the function then the interrupt is not enabled. If it did enter and returns, you'll get return status HAL_OK.
2024-01-11 12:16 AM
Just upload the whole project so we can see the actual code and the ioc file. And let us know if you're using a custom board or a Nucleo/Discovery board.
2024-01-11 12:17 AM
i will verify again , thank you for answering
2024-01-11 12:23 AM - edited 2024-01-11 12:24 AM
2024-01-11 1:19 AM
You've changed the clock settings from the default board setup. I don't have that board so I can't test if those new settings are causing an issue. Just start a new project using the default settings it creates.
2024-01-11 2:23 AM
@kkhli.1 "yhe nvic was enabled."
That's necessary - but not sufficient.
As well as having the NVIC correctly configured, you also need the UART to be correctly configured to generate interrupts.
"the uart transmit work well. but the uart recieve don't work."
Could mean that you don't have the receive interrupt enabled.
2024-01-11 6:27 AM
I have to recieve a frame from a bldc controller , this frame as follows
START CMD LENGTH BAT CUROLD TSNS STATE USER VOL CUR
| 0x66 | 0x42 | 0x?? | 1 byte | 1 byte | 2 bytes | 1 byte | 2 bytes | 2 bytes | 2 bytes |
but i didn't receive anything , the problem with how to manage the lengh of every values 's frame(byte ,2byte)could you help me please? i'm using nucleo F446RE
2024-01-11 6:42 AM
I thought you said you were abandoning this thread, and moving to your new one?
https://community.st.com/t5/stm32-mcus-products/uart-reciever/m-p/627367/highlight/true#M232225
2024-01-11 7:57 AM
That's 14 bytes but you're requesting 10 bytes. So even if you did get interrupt to work, you're going to have data out of sync.
Modify the UART1 for loopback mode and transmit to see if you receive, but in polling mode. This is to insure the rx input is not broken.
2024-01-11 8:11 AM
So reading the other posts you've created, your received data could be variable length and you're not sure how to receive the different lengths.
Use HAL_UARTEx_ReceiveToIdle_DMA or HAL_UARTEx_ReceiveToIdle_IT, and for the callback use HAL_UARTEx_RxEventCallback
Look at this project on my github which explains how to receive different lengths.
https://github.com/karlyamashita/Nucleo-G431RB_Three_UART/wiki
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.