2023-11-11 10:45 PM
hi all,
I'm Trying to send a string from STM32F401RE MCU to EPS32 Via UART i have programmed both STM as well as ESP32 and i successfully verified that data is available on UART pin of STM
Data on UART Pins of STM
But I'm not able to receive data on ESP32, i double checked the UART Hardware connection is correct
and i configured STM UART in TX_ONLY mode , did not configure any hardware flow pins ,baudrate is 9600,1 stop bit and not using parity
I'm receiving some Garbage value on Arduino
can anyone please help me with the UART message not Receiving in ESP32
Solved! Go to Solution.
2025-07-07 2:08 PM
This is some very superficial top-level initialization.
Please provide some usable context.
What Chip?
What Board?
What Pins?
What Connectivity?
How are you inspecting the output? What code moves the data from the input to the output?
You looked at the signals with a scope or anything?
2025-07-08 2:22 AM
I am using th STM32F401re board and i am trying to send the MPU6050 accelerometer values from the STm32 to the esp32 via uart6
the usart6 initalization is that i have given above and the esp32 code for the recieving i have used is
#include<HardwareSerial.h>
HardwareSerial SerialPort(2);
void setup() {
Serial.begin(115200); // Initialize the Serial Monitor for debugging
SerialPort.begin(115200,SERIAL_8N1,16,17); // Initialize the UART interface (e.g., Serial2)
}
void loop() {
if (SerialPort.available()) {
String Buffer = SerialPort.readString();
// Process the received character as needed
Serial.print("Received: ");
Serial.println(Buffer);
}}
i have connected the pc6 pin to rx2 of the esp32
2025-07-08 5:59 PM
Do your boards share a common ground? RX2 GPIO16
Data somewhat garbled, or totally?
Have you checked the signal with a scope to double check baud rate?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.