2015-03-19 4:18 AM
Hello!
I am currently using STM32F030R8T8 for communication purpose (RS485). The functions I wrote to communicate seems to be working fine but most of the time the communication stops and refuses to restart.I implemented the ''HAL_UART_ErrorCallback'' callback function to understand the bug. When the debugger stops in this callback, uart status is the following : ''HAL_UART_ERROR_FE''.
The only way I found to make the communication work again is to power off and on the microcontroller but this is not acceptable for the system I am currently developping.
My question is the following : How can I reinitialize UART softwarly from the ''HAL_UART_ErrorCallback'' callback function ?
I have already tried the following solutions but any of them are working :
-
-
Setting the error code to ''HAL_UART_ERROR_NONE''-
- Setting the uart state to ''HAL_UART_STATE_READY''
-
- Calling ''HAL_UART_DeInit'' and then ''HAL_UART_Init'' functions
About framing error :
My microcontrroller is communicating with another STM32F030R8T8 that has exactly the same program (and so, the same clocking configuration). I use internal oscillator with no PLL and the frequency is low. Can I resolve my framing error by activation the PLL to give my microcontroller more accurency (my uart baudrate is 9600) ?
#uart-framing-error-on-stm32f0-de2015-11-25 7:43 AM
Hello, On My project I found a similar situation and after +3 days debugging to find the cause and its solution, essentially I solved with:
void HAL_UART_ErrorCallback(UART_HandleTypeDef *huart)
{//I implement this .. but eventually you can decide with different approach
//Many macros/proc on this code .. is just to be a hint (mem/rec about this possibility) __HAL_UART_CLEAR_OREFLAG(huart); __HAL_UART_CLEAR_NEFLAG(huart); __HAL_UART_CLEAR_FEFLAG(huart);/* Disable the UART Error Interrupt: (Frame error, noise error, overrun error) */
__HAL_UART_DISABLE_IT(huart, UART_IT_ERR);//The most important thing when UART framing error occur/any error is restart the RX process
if(huart->Instance == USART1) { //Restarting the RX, .. 1 byte. .. u8DATUartShortRxBuffer is My own rx buffer HAL_UART_Receive_IT(huart, u8DATUartShortRxBuffer1, 1); }if(huart->Instance == USART2)
{ //Restarting the RX, .. 1 byte. HAL_UART_Receive_IT(huart, u8DATUartShortRxBuffer2, 1); }}
void MX_USART1_UART_Init(void)
{huart1.Instance = USART1;
huart1.Init.BaudRate = 115200; huart1.Init.WordLength = UART_WORDLENGTH_8B; huart1.Init.StopBits = UART_STOPBITS_1; huart1.Init.Parity = UART_PARITY_NONE; huart1.Init.Mode = UART_MODE_TX_RX; huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE; huart1.Init.OverSampling = UART_OVERSAMPLING_16; huart1.Init.OneBitSampling = UART_ONEBIT_SAMPLING_DISABLED ; huart1.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT; HAL_UART_Init(&huart1);}
/* USART2 init function */void MX_USART2_UART_Init(void)
{huart2.Instance = USART2;
huart2.Init.BaudRate = 4800; huart2.Init.WordLength = UART_WORDLENGTH_8B; huart2.Init.StopBits = UART_STOPBITS_1; huart2.Init.Parity = UART_PARITY_NONE; huart2.Init.Mode = UART_MODE_TX_RX; huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE; huart2.Init.OverSampling = UART_OVERSAMPLING_16; huart2.Init.OneBitSampling = UART_ONEBIT_SAMPLING_DISABLED ; huart2.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT; //When parity is on use, from ST forum => 8-bit + parity is configured as 9-bit in STM32 implementation. #if 0 //In some case, own ckts, is necessary a pin swap .. on My case it's disabled huart2.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_TXINVERT_INIT | UART_ADVFEATURE_SWAP_INIT; huart2.AdvancedInit.TxPinLevelInvert = UART_ADVFEATURE_TXINV_ENABLE; huart2.AdvancedInit.Swap = UART_ADVFEATURE_SWAP_ENABLE; #endif HAL_UART_Init(&huart2);}
===================================================================================================
On My case, after a power-on the reception stops on UART2, but the transition still happens.I observed:
1.) that on generated HAL codes was not including a basic code for the function void HAL_UART_ErrorCallback(UART_HandleTypeDef *huart), I put on My own module this above function; 2.) On debug mode by Keil, on TX/RX no any problem was observed when the firmware was transferred directly (F8) without a new power-on; 3.) I think that when an error occur/HAL_UART_ErrorCallback, the reception must be restarted as on HAL_UART_ErrorCallback, independentlly of the STM32 families (STM32F0x, STM32F1x, STM32F2x, STM32F3x, STM32F4, ..) 4.) On real world Common errors that can happens and eventually stops the reception/communication w/ HAL_UART_ERROR_FE, HAL_UART_ERROR_NE, errors .. be aware and implement the re-start reception as similar above (HAL_UART_ErrorCallback). #define HAL_UART_ERROR_FE ((uint32_t)0x00000004) #define HAL_UART_ERROR_NE ((uint32_t)0x00000002)Minor things that I observed:
With STM32CubeMX was configured all pin outs and generated the HAL device drivers.
After that all pin out was rightly configured I put attention to the clock sources (to be confident that clock jitter is not problem source) (for UART1 clock Mux, I'm using SYSCLK=48MHz, PLLCLK from with one crystal of 8MHz that the PLL Source Mux->HSE was adjusted to achieve the desired clock/48MHz) PLL Source Mux -> HSE, PREDiv=/1, VCOInput=8, PLLMul=x6 ..I'm using Keil MDK-ARM 5.16a IDE, as compiler tools..
Tool Version Numbers: Toolchain: MDK-ARM Professional Version: 5.16a Toolchain Path: C:\Keil_v5\ARM\ARMCC\Bin C Compiler: Armcc.exe V5.06 (build 20) Assembler: Armasm.exe V5.06 (build 20) Linker/Locator: ArmLink.exe V5.06 (build 20) Library Manager: ArmAr.exe V5.06 (build 20) Hex Converter: FromElf.exe V5.06 (build 20) CPU DLL: SARMCM3.DLL V5.16a Dialog DLL: DCM.DLL V1.13.2.0 Target DLL: STLink\ST-LINKIII-KEIL_SWO.dll V2.0.17.0 Dialog DLL: TCM.DLL V1.14.5.0STM32CubeMX 4.11.0, Firmware package for Family STM32F0 1.4.0
STM32F042C6Tx uController with LQFP48 package. UART1Tx = PIN30, UART2Rx=PIN31, UART2Tx=12 and UART2Rx=13My microcontrroller is communicating with another embedded coomunication module (RF/module) by USART2.
Eventually this info can help you or someone else/other, GregWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.