2025-07-18 5:18 AM - last edited on 2025-08-20 1:05 AM by STTwo-32
Hi,
I am working on a project and having the following problem:
My UART DMA is not working. I am transmitting a string, that should be visible in the terminal but it is not. The TX complete callback function is being triggered, so it looks like it works but there is nothing in the terminal.
Previously, I was using UART without DMA and things were working fine. It confirms that the hardware connections and the VCP connections are correctly set up.
What I have done so far:
- I enabled UART2, tested UART (without DMA). It worked well.
- I enabled DMA which gave me:
- Then I set up GPDMA1 for huart2_TX and huart2_RX. My TX configs are:
My main function:
int main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_GPDMA1_Init();
MX_ICACHE_Init();
MX_USART2_UART_Init();
/* Infinite loop */
while (1)
{
static uint32_t counter = 0;
sprintf((char *)pTxBuff, "Count: %lu\r\n", counter++);
if (huart2.gState == HAL_UART_STATE_READY) {
HAL_UART_Transmit_DMA(&huart2, pTxBuff, strlen((char *)pTxBuff));
}
HAL_Delay(1000);
}
}
Does anyone have insights into why UART2 DMA transmission is not functioning correctly and why no output is appearing on the terminal, despite the transmission complete callback being triggered?
Thanks!
2025-07-18 5:47 AM
Hello,
What product are you using and what board are you using?
2025-07-18 6:09 AM
@fa31 wrote:Previously, I was using UART without DMA and things were working fine.
If you go back to that, does it still work?
2025-07-18 6:10 AM - edited 2025-07-18 6:14 AM
I am using:
CubeMX: to generate the code Version: 6.14.1
CubeIDE: to debug the code Version: 1.18.1
Board: Nucleo WBA65RI
2025-07-18 6:12 AM
What versions?
How to write your question to maximize your chances to find a solution
2025-07-19 5:04 AM
I am using:
CubeMX: to generate the code Version: 6.14.1
CubeIDE: to debug the code Version: 1.18.1
Board: Nucleo WBA65RI
2025-07-20 7:18 AM
Yes it does. I remove the "_DMA" from the hal transmit function and I am able to send data and I can see it on the terminal.
2025-07-21 4:31 AM - edited 2025-07-22 12:33 AM
Even though I had trustzone disabled in my initial project, I noticed that trustzone option byte is enabled on my microcontroller. I tried disabling it using CubeProgrammer but was unable to do so. So instead, I generated a trustzone project with secure and nonsecure project. And now I have enabled both, the uart and DMA, on the nonsecure side. But it is still reacting the exact same way, transmit and transmit_IT works but transmit_DMA prints nothing to the terminal.
Are there any GTZS or SAU configs I need to fix? Does the DMA not working properly have something to do with the permissions around being able to access the memory?
2025-07-30 5:36 AM - edited 2025-07-30 7:11 AM
Noticed the following:
The following code does not work. It prints nothing to the terminal, but is able to trigger the callback function:
uint8_t transmission_buffer[20];
strcpy((char *)transmission_buffer, "Hello World");
HAL_UART_Transmit_DMA(&huart2, transmission_buffer, strlen((char *)transmission_buffer));
HAL_Delay(1000);While the following works perfectly:
HAL_UART_Transmit_DMA(&huart2, (uint8_t *)"Hello World", 12);
HAL_Delay(1000);
Why does the second implementation works as expected, but the first one does not produce any output?
2025-07-30 7:06 AM
In your first code, is the transmission_buffer local to a function?
If it is, it effectively ceases to exist when that function exits.
Your buffer needs to remain until the transmission completes - so make it global, or static.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.