2015-10-26 12:20 PM
Hi,
I have connected two MCU's through UART.I want to send a string from MCU 1 to MCU 2.once the MCU 1 sent the string it need to wait for some time to receive the reply from MCU 2.If MCU 1 did not get any reply from MCU 2,it need to send back a string 'u there?'How we can do this ?I have tried the following with no success :(I am really vey new for programming forgive me if you find error,uint8_t txBuffer[10] = ''HELLO\r\n''
uint8_t txBufferN[15] = ''u there ? \r\n''uint8_t rxBuffer[20] ;HAL_UART_Transmit_DMA
(&UartHandle, (uint8_t
*)txBuffer, 10);HAL_Delay(100);HAL_UART_Receive_DMA
(&UartHandle, (uint8_t
*)rxBuffer, 20);HAL_Delay(1000);if
(rxBuffer[0]=='H'
&&rxBuffer[1]=='A'
&&rxBuffer[2]=='I'
){
txBuffer[0]=
'C'
;txBuffer[1]=
'I'
;txBuffer[2]=
'A'
;txBuffer[3]=
'O'
;txBuffer[4]=
'\r'
;txBuffer[5]=
'\n'
;HAL_UART_Transmit_DMA(&UartHandle, (
uint8_t
*)txBuffer, 10);}else{HAL_UART_Transmit_DMA
(&UartHandle, (uint8_t
*)txBufferN, 15);}We’re moving the ST Community to a new platform to give you a better and more reliable community experience.