2025-02-07 1:37 PM
Basic setting of USART2: DMA Transfer and receive via interrupt as RS485.
As long as only DMA transfer is ongoing, all will be ok. At first time a receive interrupt will occur, the transmit will trigger an interrupt, even though no TXEIE is set. This crashes the system
The same settings for UART5 and USART3: there it works fine without problems (RS232 or RS485).
Whats going wrong, or some errata for this behavior?
MCU type: STM32F756
Solved! Go to Solution.
2025-02-10 11:29 PM
I got a very simple solution, but i do not understand this, why it works at the other U(S)ARTS well:
I enabled TE and UE in CR1 register at the same time in this way:
USARTx->CR1 |= (CR1_TE | CR1_UE);--> USART2 works differently to USART3 and UART5
So the handling of the control register 1 was little bit wrong, but had no influence to USART3 and UART5 but on USASRT2. murphy jokes ;-).
All U(S)ARTS work in the same (fine) way; the reference manual describes the handling in this way...
USARTx->CR1 |= CR1_TE;
USARTx->CR1 |= CR1-UE;
Thanks for your tips.
2025-02-07 4:40 PM
> DMA Transfer and receive via interrupt
If you use the "HAL" library, it can be "peculiar behavior" of the library. Do not let the system crash. Handle the interrupt and dismiss it.
2025-02-08 1:54 AM
Your own code or HAL?
The common mistake in UART interrupt handler is checking for TXE flag without checking for TXEIE. Both should be set to execute the TXE handler path.
2025-02-09 11:41 PM
Hi @rodi66
What makes you think the source for the unexpected interrupt is TXE ? is it because TXE flag is 1 in ISR ?
By the way, at end of transmission, TXE will stay at 1 and cannot be cleared in ICR, but this should not trigger USART2 interrupt.
What is USART2 ISR register content when this unexpected interrupt occurs ?
Regards
2025-02-10 1:11 AM
That ist not the case: i check the flags proper. After setting the CR1 Bits in a little different way, the sytem works fine. Unfortunately, setting brakepoint s in the interrupt handler also led to confusion in the ISR bits.
2025-02-10 1:13 AM
The TXE bit was set and the TC Bit was cleared. But no TXEIE or TXIE bit is set in the CR1 register.
2025-02-10 3:09 PM - edited 2025-02-10 3:15 PM
This is OK. TXE indicates that the transmit buffer register USART_TDR is empty (all bits shifted out). It can be empty even when TXEIE is not set.
2025-02-10 6:08 PM
The interrupt enable (IE) simply determines what gates from the status register into the NVIC
TXE can be high regardless, even if you don't have data ready to send.
2025-02-10 11:29 PM
I got a very simple solution, but i do not understand this, why it works at the other U(S)ARTS well:
I enabled TE and UE in CR1 register at the same time in this way:
USARTx->CR1 |= (CR1_TE | CR1_UE);--> USART2 works differently to USART3 and UART5
So the handling of the control register 1 was little bit wrong, but had no influence to USART3 and UART5 but on USASRT2. murphy jokes ;-).
All U(S)ARTS work in the same (fine) way; the reference manual describes the handling in this way...
USARTx->CR1 |= CR1_TE;
USARTx->CR1 |= CR1-UE;
Thanks for your tips.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.