2025-01-07 9:48 PM - last edited on 2025-01-07 11:28 PM by Peter BENSCH
Hi, I am working on an IR remote using STM32L412RBT6P. I have the touch sensing system working to provide the buttons for the user. The user touches a button to send an IR (RC5) code and an LED flashes to let you know it happened.
Q1:I have one touch channel that holds the pressed condition for 2 to 3 times longer than the the others. You can clearly see this in Cube Monitor when looking at the Delta's. You can see the channel 3 (Red) is holding the touched condition longer in the attached image. All touches are as similar as I can do. All sensors and PCB tracks are very similar to each other. What effects the duration of the touched condition?
This channel is connected is TSC_G2_IO1 (PB4). After laying out the PCB I discovered UM1913. This recommends PB4 is only used for the active shield, which I have allocated to TSC_G1_IO1, Shield and IO3, Capacitor. Does this contribute to the longer touched time?
Q2: I am currently running the clock at 20MHz. If I reduce it 2MHz to get into Low Power Run Mode are there any issues with the touch system I need to be aware of?
I recall reading the clock should not be too high for the TSC, have found no recommendations about the lower frequencies.
Any advice gratefully appreciated.
Thanks in advance, Lance.
Solved! Go to Solution.
2025-01-13 12:57 AM
Hello Lance,
Yes PB2 should be used as either an active shield or sampling capacitance only depending on the package you have and that is why you see a longer pulse.
For the 2Mhz you should be fine
Regards,
Stassen
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-01-13 12:57 AM
Hello Lance,
Yes PB2 should be used as either an active shield or sampling capacitance only depending on the package you have and that is why you see a longer pulse.
For the 2Mhz you should be fine
Regards,
Stassen
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-01-13 2:31 PM
Thanks Stassen, the new board is be made now. I hope to report back the problem is solved and I have not added any problems soon.
Regards, Lance.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.