2012-09-16 10:12 PM
Hello every1,
I've been using the keil MDK compiler for a long time. Due to some circumstances i have to use Altium Tasking toolset. As i was trying to compile one of the peripheral example(Flash Program) i got the following errors 1. lkarm E108: multiple definitions of symbol ''_START'' in both ''cstart.obj'' and ''cstart_thumb2.obj'' 2. amk E452: target 'FLASH_Program.abs' returned exit code 1 These errors remains the same for any example program. But i did not get these error when i used Keil MDK. Any hep wud be appreciated. FYI: Im using STM32F4 discovery board. #wait-for-you--clive1-!-!-!2012-09-17 7:55 AM
I'm not a TASKING guy, but the errors are related.
The second is from the make process complaining that the linker didn't build a file. The first is from the linker, and suggests your project is pulling in two copies of the start up code, either the processor's or the C runtime's. You should review the project and see if it refers to different startup_stm32xxx.s type files, or compiler command line options to use specific or default objects/libraries that contain alternative startup code. This error indicates a fatal condition, thus no output file was generated, consequently causing the second error. So basically review the files that make up the project, and then look at the meta-data which defines the settings, controls, paths, and libraries used by the compilers, assemblers and linkers.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.