STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Is 2048 points 32-bit FFT on STM32L1 real?

Posted on September 17, 2012 at 09:42Hi everybody!I'm going to use STM32L152RD in my project. The MCU has 384kb of Flash and 48kb of RAM memory (maximum for this series). And I need to perform FFT for the 3-channel signal, sampled at 2000 Hz with 24...

foruvarov by Associate II
  • 2006 Views
  • 3 replies
  • 0 kudos

STM32F207 and PHY Micrel KSZ8051RNL

Posted on September 17, 2012 at 15:16Hello, I want to use the quite new and very cheap Micrel KSZ8051RNL in RMII mode with STM32F207 in a mid volume design. Looking at Micrel's site I found and errata regarding the 8051 phy with the following note :...

abrous3d by Associate II
  • 663 Views
  • 0 replies
  • 0 kudos

How can i learn STM32f4

Posted on September 14, 2012 at 18:57Hello every one I was starting work with STM32f4 few days ago and i want to know is there any user manual for explain the all part of this device? or i have to starting with try and error with the example.Thank y...

imanpakii by Associate III
  • 2861 Views
  • 8 replies
  • 0 kudos

STM32 I2C PROBLEM

Posted on September 02, 2012 at 16:57Hello ,              I am developing firmware for  an application , in which a  24 series eeprom and   a GPS module is connected to same I2C bus of stm32l151 ,  stm32 will  receive  data from GPS  as ''SLAVE ( DE...

akp25i by Associate II
  • 3282 Views
  • 7 replies
  • 0 kudos

Controlling DMA clock in regular simultaneous ADC

Posted on September 14, 2012 at 03:36Dear colleagues,         The CPU is an STM32F407IG, and I am using the standard peripheral libraries for STM32F4xx (both answers in the context of the library or the registers directly are appreciated).         I...

Troubleshooting a Hard Fault

Posted on September 15, 2012 at 17:52 I am attempting to buid an ARM-GCC/Eclipse build environment from scratch. I'm beginning to realize that this is a bigger task than I'd first thought. In any case, I was able to build the STM32F0 dem...

Interface STEVAL-mki062v2 to STM32VLDISCOVERY

Posted on September 13, 2012 at 19:10I apologize right now for my English. I purchased a STM32VLDISCOVERY and unsteval-mki0 +2 v2 both st microelectronics. I tried the program that is given with the second component, and seemed very nice. Wanted ho...

nico23 by Senior III
  • 2311 Views
  • 5 replies
  • 0 kudos

communicate with PC

Posted on September 13, 2012 at 22:30I started learn about STM32f4 discovery and i want to send and receive some data between my discovery board and my PC before i was working with AVR and i was sending and receiving data with RS232 but now i want t...

imanpakii by Associate III
  • 916 Views
  • 3 replies
  • 0 kudos

ADC value in interrupt

Posted on September 14, 2012 at 14:42I have set up interupts on the ADC1 (AWD) and ADC2(EOC). They both works well, but i'm having some concern about the values from the ADC1. If I get an AWD interrupt, how can I then make sure that I'm getting the ...

oe2 by Associate III
  • 677 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.