2011-02-10 7:10 AM
Trouble, need urgent help.
2011-05-17 5:24 AM
1. Have you enabled a clock to the timer anywhere like
RCC_APB1PeriphClockCmd (RCC_APB1Periph_TIM6, ENABLE); 2. Have you named an IRQ handler right?void TIM6_IRQHandler(void){
...
} 3. Have you added the correct startup file to the project? For instance, ''startup_stm32f10x_hd.s''. Look inside your startup file: can you find a line ''TIM6_IRQHandler'' there?
2011-05-17 5:24 AM
Attach the application's HEX file.
2011-05-17 5:24 AM
Yes, I have checked all your points.
And the application works fine when located at 0x0800 0000. And I have also move the interrupt vector table using: NVIC_SetVectorTable(NVIC_VectTab_FLASH, 0x8100); It's so stange. No I have also found when the MCU receives a byte on UART5 I get a Bus Fault exception (a jump to BusFault_Handler(). I have looked at the memory addresses for these interrupt vectors and they are correct. I use a STM32F103ZET6 device. Is there any chip errata on this?2011-05-17 5:24 AM
Here is the application hex file that I'm experimenting right now to find the problem.
It is located from 0x08008100. I have scaled away all other code. It only does the following: int main(void) { TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure; NVIC_InitTypeDef NVIC_InitStructure; NVIC_SetVectorTable(NVIC_VectTab_FLASH, 0x8100); // System clocks configuration SystemInit(); // Enable clocks //RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA1, ENABLE); //RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA2, ENABLE); RCC_APB1PeriphClockCmd(RCC_APB1Periph_PWR | RCC_APB1Periph_BKP | //RCC_APB1Periph_SPI2 | //RCC_APB1Periph_SPI3 | //RCC_APB1Periph_CAN1 | //RCC_APB1Periph_USART2 | //RCC_APB1Periph_USART3 | //RCC_APB1Periph_UART4 | //RCC_APB1Periph_UART5 | //RCC_APB1Periph_TIM2 | //RCC_APB1Periph_TIM3 | //RCC_APB1Periph_TIM4 | //RCC_APB1Periph_TIM5 | RCC_APB1Periph_TIM6 //RCC_APB1Periph_TIM7 | //RCC_APB1Periph_I2C1 , ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA | RCC_APB2Periph_GPIOB | RCC_APB2Periph_GPIOC | RCC_APB2Periph_GPIOD | RCC_APB2Periph_GPIOE | RCC_APB2Periph_GPIOF | RCC_APB2Periph_GPIOG | //RCC_APB2Periph_USART1 | //RCC_APB2Periph_ADC1 | //RCC_APB2Periph_ADC2 | //RCC_APB2Periph_ADC3 | RCC_APB2Periph_AFIO, ENABLE); // Enable CAN RX0 interrupt IRQ channel NVIC_InitStructure.NVIC_IRQChannel = TIM6_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); // ======================================================================== // Configure TIM6 // // Generate a timer interrupt 6 times per period // Time base configuration TIM_TimeBaseStructure.TIM_Period = 59999; // Period 60000 = 3.3333 ms TIM_TimeBaseStructure.TIM_Prescaler = 3; // Divide 72MHz with 4 = 18MHz TIM_TimeBaseStructure.TIM_ClockDivision = TIM_CKD_DIV1 ; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM6, &TIM_TimeBaseStructure); // Clear interrupt flags TIM6->SR = 0x0000; // TIM IT enable TIM_ITConfig(TIM6, TIM_IT_Update, ENABLE); // Enable timer TIM6->CR1 |= TIM_CR1_CEN; } If i disable the last row (not enabling timer 6) it doesn't fail. But as soon as I activate the timer 6 a Usage Fault exception occurs.2011-05-17 5:24 AM
Dear SirM,
Your trouble are due to the fact that your application start boundary is not multiple of 0x200 : ''0x08008100''. Please move it to be at ''0x08008200''. Have a look on our : Page 133 : ''you must align the offset to the number of exception entries in the vector table. The minimum alignment is 128 words'' , word is 32-bits that means 128 x 4 = 512 Bytes . This is mainly due to the Vector table size of our High-density devices2011-05-17 5:24 AM
Your TIM6 interrupt doesn't seem to do much, just increment a RAM variable and leave. It does not appear to actually clear any interrupt, so it will get stuck there endlessly as it repeatedly tail-chains.
Be aware also that SystemInit() is already called before it executes main() 08008354 SUB16 TIM6_IRQHandler: 08008354 B480 push {r7} 08008356 AF00 add r7, sp, #0 08008358 F240 0300 movw r3, #0 ; $0 0800835C F2C2 0300 movt r3, #8192 ; $2000 08008360 681B ldr r3, [r3, #0] 08008362 F103 0201 add.w r2, r3, #1 ; $1 08008366 F240 0300 movw r3, #0 ; $0 0800836A F2C2 0300 movt r3, #8192 ; $2000 0800836E 601A str r2, [r3, #0] 08008370 46BD mov sp, r7 08008372 BC80 pop {r7} 08008374 4770 bx lr Translates roughly to : int foo; void TIM6_IRQHandler(void) { foo++; }2011-05-17 5:24 AM
Thank you very much. I will try that tomorrow.
I have not used high density STM32's until now so I was unaware of that.Learning all the time.
2011-05-17 5:24 AM
In the real application I do in fact have a:
TIM6->SR = 0x0000;
, at the entry of the interrupt handler.
I managed to scale away too much when I posted my test code. ;)
And the counter was just to see if the interrupt handler had activated.
2011-05-17 5:24 AM
When I look at the function header for the NVIC_SetVectorTable() function in misc.c in ST Libraries it says:
@param Offset: Vector Table base offset field. This value must be a multiple of0x100
. There should be some note about this pitfall here?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.