2017-05-04 11:07 PM
Dear All,
I am looking for some support in verifying our transformer design as i am having some trouble in generating the output and i have doubts on the transformers we already have.
>
> Processor used : STM32F407
>
> Use case : 48 V DC on the transformer primary is switched by the controller to generate 1600 V Peak to Peak output on the secondary in 160KHz frequency.
>
> Issue : When the transformer is loaded, the clock of the STM controller changes and there seems to be some disturbance to the power section too.
> When the primary voltage is reduced from 48V to a lessor voltage like 5V-12V, depending on the board, this works as expected with lessor output P2P in the secondary.
Please help me to resolve the issue.
Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.