2023-11-02 1:56 AM - edited 2023-11-02 3:03 AM
I do not see any information on the datasheet or reference manual, how is the TRACECLK in STM H5 (particularly 563 if it matters) derived ? Is the TRACECLKIN SYSCLK or FCLK ?
Solved! Go to Solution.
2023-11-02 6:33 AM
Hello @mete,
TRACECLK is connected to SYSCLK/2. Thus, max frequency is 125MHz.
Kind Regards,
Gwénolé
2023-11-02 6:33 AM
Hello @mete,
TRACECLK is connected to SYSCLK/2. Thus, max frequency is 125MHz.
Kind Regards,
Gwénolé
2023-11-02 6:46 AM
Thanks @GwenoleB
2024-12-17 7:17 PM
Is this relationship between TRACECLK and SYSCLK documented in the reference manual? I haven't seen a fixed clock divider mentioned in the documentation or STMCubeMX yet.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.