2009-05-02 3:28 AM
Timers in quadrature decoder mode
2011-05-17 4:10 AM
Hmm, after reading the data sheet, it seems that there's no pin for TIM2_CH1..
Is there a way to use CH3 / CH4 instead?!2011-05-17 4:10 AM
Hi!
I want to use an STM32F103ZE to control a 4 axis CNC machine (with DC servos and quadrature encoders). As I understand, I can use TIM2..5 to simultaneously capture the 4 encoder positions, but I wonder which pins to use. Would this be ok? : TIM2_CH1 Enc. 1 Phase A TIM2_CH2 Enc. 1 Phase B TIM3_CH1 Enc. 2 Phase A TIM3_CH2 Enc. 2 Phase B TIM4_CH1 Enc. 3 Phase A TIM4_CH2 Enc. 3 Phase B TIM5_CH1 Enc. 4 Phase A TIM5_CH2 Enc. 4 Phase B The Reference Manual is a little bit unclear here. Can the other timer channels 3/4 also be used for quadrature capture?! Or do I have to use TIMx_CH1/2? What do the signals TI3FP3, TI3FP4, TI4FP3 and TI4FP4 on page 270 do?! I can't find any other reference to them in the manual.. Also, the firmware library seems to lack an example program for quadrature capture. Greetings from Germany, Thomas KindlerWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.