2015-07-05 8:19 PM
Timer works in Input capture mode. It captures period of rectangular wave. I would like to get interrupt on each eighth front, but interrupt does not dependent of prescaler. Controller: stm32f030f6p6. There is code fragment indicatind problem.
&sharpdefine TIMER_TEMP TIM2&sharpdefine TIMER_HUM TIM3&sharpdefine GET_PERIOD_TEMP (TIM_GetCapture2(TIMER_TEMP))&sharpdefine GET_PERIOD_HUM (TIM_GetCapture1(TIMER_HUM))int temp = 0;int hum = 0;void PeriphInit(void){ GPIO_InitTypeDef gpio; TIM_TimeBaseInitTypeDef tim; TIM_ICInitTypeDef timIn; NVIC_InitTypeDef nvic; RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2 | RCC_APB1Periph_TIM3, ENABLE); RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE); GPIO_StructInit(&gpio); gpio.GPIO_Pin=GPIO_Pin_1; gpio.GPIO_Mode=GPIO_Mode_AF; gpio.GPIO_Speed=GPIO_Speed_50MHz; gpio.GPIO_OType = GPIO_OType_PP; gpio.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOA,&gpio); GPIO_PinAFConfig(GPIOA, GPIO_PinSource1, GPIO_AF_2); TIM_TimeBaseStructInit(&tim); tim.TIM_Prescaler = (SystemCoreClock/12000000)-1; tim.TIM_Period = 0xFFFFFFFF; tim.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIMER_TEMP, &tim); timIn.TIM_Channel = TIM_Channel_2; timIn.TIM_ICPolarity = TIM_ICPolarity_Rising; timIn.TIM_ICSelection = TIM_ICSelection_DirectTI; timIn.TIM_ICPrescaler = TIM_ICPSC_DIV4;//This prescaler doesn't work timIn.TIM_ICFilter = 0x0; TIM_SelectInputTrigger(TIMER_TEMP, TIM_TS_TI2FP2); TIM_SelectSlaveMode(TIMER_TEMP, TIM_SlaveMode_Reset); TIM_PWMIConfig(TIMER_TEMP, &timIn); TIM_SetCounter(TIMER_TEMP, 0); nvic.NVIC_IRQChannel=TIM2_IRQn; nvic.NVIC_IRQChannelPriority = 0; nvic.NVIC_IRQChannelCmd = DISABLE; NVIC_Init(&nvic); NVIC_EnableIRQ(TIM2_IRQn); TIM_ITConfig(TIMER_TEMP, TIM_IT_CC2, ENABLE); TIM_Cmd(TIMER_TEMP, ENABLE);}void TIM2_IRQHandler(){ temp = GET_PERIOD_TEMP; TIM_ClearITPendingBit(TIMER_TEMP, TIM_FLAG_CC2);}int main(){ PeriphInit(); while (1);} #timerWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.