2026-04-23 11:09 AM - last edited on 2026-04-29 2:36 AM by Andrew Neil
Hello,
I used MX2 for the last two weeks and it is a great improvement over MX. I build many small projects with it and I am constantly running into a problem related to timer configuration. I enter the values for the Prescaler and the Counter period as Integers and unfortunately when I close the project and reopen MX2 converts the value to Hex (and indicates that it is a Hex value). I keep forgetting that MX2 does this and I enter a new value as an Int thinking that my selection was sticky. Could you make the Int/Hex selection sticky? It's a small issue but it will save developers some trouble.
Thank you,
Gil
2026-04-24 12:30 AM
Hello @gil_dobjanschi ,
Love this feedback, and thanks for calling it out.
You are right, the Int/Hex choice should stay where you left it when you reopen a project. That would avoid exactly the kind of small, repeated mistake you described.
We will add it to the list of UX Improvements!
Thank you,
Mads
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.