2019-11-09 9:36 AM
Hi,
I want to use output compare4 mode for timer 4. I have doubt regarding the register
setting in TIM4->CCMR2 value
As per the reference manual it is given
Bits 14:12 OC4M: Output compare 4 mode and
Bit 11 OC4PE: Output compare 4 preload enable
I have to set this bits.
TIM4->CCMR2 = 0x6800; //0b 0110 1000 0000 0000
IM4->CCMR2 = 0x7800; Which one is correct?
Is this value correct?
0b 0110 1000 0000 0000
and in the reference manual there is no description for the 12, 13 and 14 bits. If it is there, how to set them?
Solved! Go to Solution.
2019-11-09 10:06 AM
2019-11-09 10:06 AM
Have a look at the description of OC1M bits in CCMR1.
JW
2019-11-09 10:08 AM
Thanks for the reply.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.