2008-03-25 10:29 PM
timer 1 with external clock
2011-05-17 3:27 AM
hello ,
i tried to work with timer 1 with external clock of 2 hz. the source clk is 1 second pulse on and 1 second off. the problem is that the interrupt excute every 3 pulses (6 SECONDS) and not every 2 seconds. (2 pulses delays). my configuration is below. what did i worng? /* Enable the TIM1 UP Interrupt */ NVIC_InitStructure.NVIC_IRQChannel = TIM1_UP_IRQChannel; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 1; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 3; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); /***config TIM1 for priod 1 time and autorload of 1 ******/ TIM1_TimeBaseStructInit(&TIM1_TimeBaseStructure); TIM1_OCStructInit(&TIM1_OCInitStructure); TIM1_TimeBaseStructure.TIM1_Prescaler = 0; TIM1_TimeBaseStructure.TIM1_CounterMode = TIM1_CounterMode_Down; TIM1_TimeBaseStructure.TIM1_Period = 0x1; TIM1_TimeBaseStructure.TIM1_ClockDivision = 0x0; TIM1_TimeBaseStructure.TIM1_RepetitionCounter = 0x0; TIM1_SetAutoreload(0x1); TIM1_TimeBaseInit(&TIM1_TimeBaseStructure); /**********************************************************************/ /************config external clock without presclar and rising edge*****/ TIM1_ETRClockMode2Config(TIM1_ExtTRGPSC_OFF, TIM1_ExtTRGPolarity_NonInverted, 0x0); /************config PE7 AS ETR for TIM1****************************/ GPIO_PinRemapConfig(GPIO_FullRemap_TIM1, ENABLE); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_7 ; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IPU; GPIO_Init(GPIOE, &GPIO_InitStructure); /**********ENABLE INTERRUPT****************************************/ TIM1_ITConfig(TIM1_IT_Update, ENABLE); TIM1_Cmd(ENABLE);2011-05-17 3:27 AM
I can't understand your post:
''i tried to work with timer 1 with external clock of 2 hz. the source clk is 1 second pulse on and 1 second off.'' then it's 0.5Hz, not 2Hz. which is it? ''the problem is that the interrupt excute every 3 pulses (6 SECONDS) and not every 2 seconds. (2 pulses delays).'' if you want an interrupt on every external pulse why are you using a timer? you need an EXTI line.2011-05-17 3:27 AM
thanks for your remarks.
the external clk is 2 hz (1 sec on and 1 off). and i the problem that the interrupt happen every 3 rise edge and not every rise edge as i expected. for your question: yes it is possible to do this also with EXTI . for our application we supply the same clock source (our clock source is very slow 2 hz)to some devices in order to synchronize between them and to do some operations simultaneous.2011-05-17 3:27 AM
hi,
if the period is 2 seconds (1 on, 1 off) the frequency (1/T) is 0.5 Hz, not 2. forget the timer, use an EXTI. using a timer with a period of 1 count (that is, a constant value) is a corner case and is never recommended; and besides you don't need it. many timers misbehave in this condition. in particular, I'm remembering one of the PICs or dsPICs with motor control: in this chip, if you set the period to 1 you'll enter the counter in an invalid state from which you can't recover by software, but only with a reset (the shadow reg is never updated again). without going to that extreme, many timers don't fire the events correctly in this condition. I don't see why you want a timer, please explain if you continue to do so.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.